2011-09-30 04:41:33     U-boot stops after returning from console_init_r

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

2011-09-30 04:41:33     U-boot stops after returning from console_init_r

Michal Koziel (NORWAY)

Message: 103651   

 

U-boot stops after returning from console_init_r , never reaches main_loop. What happens in between? 

 

How to debug this?

 

Output:

 

 

 

Net: Hit any key to stop autoboot: 0

THOR> loadb

## Ready for binary (kermit) download to 0x01000000 at 57600 bps...

## Total Size = 0x0002ae58 = 175704 Bytes

## Start Addr = 0x01000000

THOR> go 0x1000000

## Starting application at 0x01000000 ...

ABabCabcdghijDabchij?!kž  µ‹”\§ ‡T«„¥®½Qü

 

U-Boot 2010.06 (ADI-2010R1-RC2) (Sep 30 2011 - 10:23:54)

 

CPU: ADSP bf537-0.3 (Detected Rev: 0.3) (spi flash boot)

Board: BF537 Thor board

Clock: VCO: 500 MHz, Core: 500 MHz, System: 100 MHz

RAM: 64 MiB

Flash: ## Unknown FLASH on Bank 1 - Size = 0x00000000 = 0 MB

0 Bytes

SF: Detected M25P64 with page size 256, total 8 MiB

*** Warning - bad CRC, using default environment

 

In: serial

Out: serial

Err: serial

 

 

 

 

 

 

 

 

 

QuoteReplyEditDelete

 

 

2011-09-30 04:46:52     Re: U-boot stops after returning from console_init_r

Michal Koziel (NORWAY)

Message: 103653   

 

I found what is going on i between and start digging into this. Any help is welcome

QuoteReplyEditDelete

 

 

2011-09-30 05:05:56     Re: U-boot stops after returning from console_init_r

Aaron Wu (CHINA)

Message: 103654   

 

Are you using the ADI default u-boot release or you have changed something, what's your hardware board, an ADI board or customer board?

QuoteReplyEditDelete

 

 

2011-09-30 05:35:35     Re: U-boot stops after returning from console_init_r

Michal Koziel (NORWAY)

Message: 103655   

 

It's a custom board based on the BF537-stamp board.

 

I have undefined CONFIG_MISC_INIT_R and u-boot botted up.

 

I will now check what is wrong with misc_init_r

Attachments

    Outcomes