2011-05-24 14:16:49     [GIT] U-Boot and BUILD-RELEASE

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

2011-05-24 14:16:49     [GIT] U-Boot and BUILD-RELEASE

James Kosin (UNITED STATES)

Message: 100815   

 

BUILD-RELEASE seems to be broken in the latest GIT head.  It fails to find and compile init.S.  So the u-boot-.elf files are not created.  I've commented the section that tests for initelf and builds the extra loads.  I'm sure someone else will be complaining; but, wasn't sure if this was a BUG.

 

Thanks,

 

James

QuoteReplyEditDelete

 

 

2011-05-24 15:14:13     Re: [GIT] U-Boot and BUILD-RELEASE

Mike Frysinger (UNITED STATES)

Message: 100816   

 

i dont directly run that script until it's release time, so failures can sometimes go unnoticed.  ive fixed this up now to use the new init.elf location ... thanks!

QuoteReplyEditDelete

 

 

2011-05-25 09:26:35     Re: [GIT] U-Boot and BUILD-RELEASE

James Kosin (UNITED STATES)

Message: 100836   

 

Thanks, the patch fixes the issue.

 

I use the script all the time; because it makes building the two different versions of u-boot I need go easier.  I had to comment out all the other models; but, it makes buidling for uart and spi-master easy without having to compile two separate builds.  I also have it build for the bf537-stamp if I ever need to go back and test with that board as well.

 

James

Attachments

    Outcomes