2011-04-06 15:53:22     JTAG Programmer for S25FL128P

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

2011-04-06 15:53:22     JTAG Programmer for S25FL128P

Blair Fredericks (CANADA)

Message: 99631   

 

Hi,

 

We have a custom bf561 board, I have tried programming our SPI Flash from Spanison it is the S25FL128P

 

using the ICEBear Classic In Circuit Programmer, it appear this device at this time is not supported.

 

I have looked at the Programmer from Danville Signal, the SPI Flash we have on board is not support for the BF561.

 

Does anyone know what JTAG ICE Programmer I can use to program our flash with U-Boot and uClinux?

 

WIl Analog Devices ADZS-ICE-100B program the S25FL128P?

 

Does or Has anyone programmed this IC before with a JTAG Programmer and if so which one?

 

Thanks,

 

Blair

QuoteReplyEditDelete

 

 

2011-04-06 18:42:40     Re: JTAG Programmer for S25FL128P

Mike Frysinger (UNITED STATES)

Message: 99632   

 

you could load u-boot over jtag and let it do the SPI programming

QuoteReplyEditDelete

Attachments

    Outcomes