2011-03-24 10:59:06     BF506F-EZKIT

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

2011-03-24 10:59:06     BF506F-EZKIT

Lars Weber Rasmussen (DENMARK)

Message: 99217   

 

Hi!

 

RE: u-boot-trunk

 

I have tried to build and flash u-boot into BF506F-EZKIT, using VDSP++ flashprogrammer.

 

It does not start up automatically, but changing PC ( in VDSP )  to 0xffa00000 and then <F5> starts it up. I guess I am missing something... please help with instruction how-to get started.

 

 

 

br

 

lars

QuoteReplyEditDelete

 

 

2011-03-24 20:20:51     Re: BF506F-EZKIT

Mike Frysinger (UNITED STATES)

Message: 99222   

 

honestly, the bf506-ezkit port atm is more of a PoC.  it takes up a good chunk of on-chip SRAM atm.  30KiB of ISRAM and 12KiB of DSRAM.

QuoteReplyEditDelete

 

 

2011-03-25 11:27:59     Re: BF506F-EZKIT

Lars Weber Rasmussen (DENMARK)

Message: 99257   

 

Hi Mike!

 

In VDSP, application is split into a static part ( flashed into executable FLASH ) and a loader part which gets booted after a reset. If you are prepared to give up the 'update' command u-boot can still be used to boot or call ( not linux of course ) other applications.

 

I use u-boot on other platforms to boot VDSP applications. It works nice and u-boot can be used to upgrade your firmware in the field.

 

I have an idea to use uboot to calibrate a BF based smart sensor after the PCB has been molded into a metal can.

 

Using u-boot will save me some programming hours.

 

I still wonder why u-boot does not start running after it has been loaded.

 

Any idea why? A missing flag in the loader file header?

 

br/ lars

Attachments

    Outcomes