2011-01-07 17:12:57     Upgrading U-Boot docs refer to eeprom command

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

2011-01-07 17:12:57     Upgrading U-Boot docs refer to eeprom command

Matt Prewett (UNITED STATES)

Message: 97259   

 

I was reading through the the "Upgrading U-boot" documentation at the following URL:

 

http://docs.blackfin.uclinux.org/doku.php?id=bootloaders:u-boot:upgrading

 

 

 

and noticed the following:

 

*****************

 

Serial NOR flash

 

Updating serial flash is much more straight forward. The eeprom command will take care of erasing/writing sectors.

 

*****************

 

 

 

I don't see the "eeprom" command in the latest u-boot release.  I think it uses the "sf" commands instead.

 

-Matt

QuoteReplyEditDelete

 

 

2011-01-07 17:24:51     Re: Upgrading U-Boot docs refer to eeprom command

Mike Frysinger (UNITED STATES)

Message: 97260   

 

eeprom isnt enabled in our releases, but it still exists in the source.  ive changed the docs from "eeprom" to "sf" to reflect all the ADI boards.

QuoteReplyEditDelete

Attachments

    Outcomes