2011-01-07 11:56:23     u-boot.hex not being created

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

2011-01-07 11:56:23     u-boot.hex not being created

Matt Prewett (UNITED STATES)

Message: 97256   

 

I have installed the latest toolchain on Ubuntu 10.04 and am able to compile u-boot.

 

 

 

The following page implies that a u-boot.hex file will be created during compilation:

 

http://docs.blackfin.uclinux.org/doku.php?id=bootloaders:u-boot:compiling

 

 

 

I see u-boot.bin, u-boor.ldr, and u-boot.srec but no u-boot.hex. Did you all change the build environment to not create the u-boot.hex file?

 

 

 

BTW: I was able to create this manually using the command in the above document.

 

-Matt

QuoteReplyEditDelete

 

 

2011-01-07 12:21:33     Re: u-boot.hex not being created

Mike Frysinger (UNITED STATES)

Message: 97257   

 

ive fixed the documentation.  .hex files are not necessary for VDSP flashing.

 

QuoteReplyEditDelete

Attachments

    Outcomes