2010-11-11 21:59:58     Uboot and flash address

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

2010-11-11 21:59:58     Uboot and flash address

Chen Kuantong (CHINA)

Message: 95787   

 

I need to program "uboot.bin" on the flash of bf561,but I am not sure where this file should be programmed. Whether I need to program from 0x0000 0000?

QuoteReplyEditDelete

 

 

2010-11-11 22:13:23     Re: Uboot and flash address

Mike Frysinger (UNITED STATES)

Message: 95788   

 

address 0 is sdram.  0x20000000 is the start of the async banks where the flash is connected.

QuoteReplyEditDelete

 

 

2010-11-24 07:52:47     Re: Uboot and flash address

Chen Kuantong (CHINA)

Message: 96174   

 

Thanks for your reply.

 

I finnally get it,.

 

When reset the board of ezkit533, the PC address is 0x20000000, that is the very starting address of flash.

 

So, when I use the VDSP to program the u-boot on flash, the staring offset address should be 0x00000000(exactly the start of flash).

QuoteReplyEditDelete

Attachments

    Outcomes