2009-10-01 18:03:05     compile problem:No rule to make target `.depend

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

2009-10-01 18:03:05     compile problem:No rule to make target `.depend

Doug Bailey (UNITED STATES)

Message: 80782   

 

I am having a problem building u-boot 1.1.6 for my bf527 based board.  I have

setup the configuration of my board using the guidlines listed at:

 

http://docs.blackfin.uclinux.org/doku.php?id=bootloaders:u-boot:porting

 

Further, I have based my build using the bf527-ezkit as a template.

 

I have been able to build my image until I recently upgraded my Ubuntu 9.04

based system with the latest update package.  Now when I build, the following

message appears when the build terminates.:

 

make[1]: Leaving directory `/usr/src/dasboot/u-boot-1.1.6/lib_generic'

make -C board/superboard/

make[1]: Entering directory `/usr/src/dasboot/u-boot-1.1.6/board/superboard'

make[1]: *** No rule to make target `.depend', needed by `libsuperboard.a'.Stop.

make[1]: Leaving directory `/usr/src/dasboot/u-boot-1.1.6/board/superboard'

make: *** [board/superboard/libsuperboard.a] Error 2

 

I can build the bf527-ezkit variant without any problems.

 

Any suggestions where I need to look?

 

Thanks

 

Doug Bailey

QuoteReplyEditDelete

 

 

2009-10-01 18:34:31     Re: compile problem:No rule to make target `.depend

Mike Frysinger (UNITED STATES)

Message: 80784   

 

did you create a superboard.c file like the docs said ?

QuoteReplyEditDelete

 

 

2009-10-02 09:31:25     Re: compile problem:No rule to make target `.depend

Doug Bailey (UNITED STATES)

Message: 80804   

 

Yes.

 

As I also mentioned, I have previously compiled the superboard project successfully.  It has only been since an upgrade of my environment that the compilation has failed.

 

What I don't know is where I need to be looking to find out why the .depend rule is not being found. 

QuoteReplyEditDelete

 

 

2009-10-02 12:21:46     Re: compile problem:No rule to make target `.depend

Mike Frysinger (UNITED STATES)

Message: 80808   

 

look at the Makefile in the superboard dir and make sure every object listed has a proper source file

QuoteReplyEditDelete

 

 

2009-10-14 14:19:11     Re: compile problem:No rule to make target `.depend

Doug Bailey (UNITED STATES)

Message: 81212   

 

Sloppy on my part. I forgot to check a file into svn and a subsequent checkout did not have the necessary source.

 

I should have caught that before posting here.  Sorry to waste your time.

 

Thanks for the support,

 

Doug

Attachments

    Outcomes