2010-10-13 09:53:51     JFFS2 Access in UBOOT from a serial Flash device

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

2010-10-13 09:53:51     JFFS2 Access in UBOOT from a serial Flash device

Patrick Sestier (CANADA)

Message: 94473   

 

I would like to access a JFFS2 file system at boot time and boot a custom ldr image.

 

The flash device I am using is a M25P64 serial flash.

 

After some reading of the source code, it seems that the JFFS2 support in u-boot mostly uses parrallel flash.

 

Is it possible to get JFFS2 working with a serial flash device in uboot?

QuoteReplyEditDelete

 

 

2010-10-13 09:57:17     Re: JFFS2 Access in UBOOT from a serial Flash device

Mike Frysinger (UNITED STATES)

Message: 94475   

 

atm, i dont believe so -- this applies to all serial flashes (SPI)

QuoteReplyEditDelete

Attachments

    Outcomes