2010-10-12 22:20:21     SMC91111: PHY auto-negotiate timed out

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

2010-10-12 22:20:21     SMC91111: PHY auto-negotiate timed out

Rui Guo (CHINA)

Message: 94447   

 

Hi,

 

I work with bf561-ezkit , the revisions are:

 

1.       Silicon revision:skbcz-6v

 

2.       Board Revision:2.3

 

3.       BOM:3.2

 

have a usb-lan board connected on the main board.

 

after doing a "ping" command, I got this output:

 

bfin> ping 192.168.0.2

SMC91111: PHY auto-negotiate timed out

Using MAC Address 10:00:00:11:10:00

ping failed; host 192.168.0.2 is not alive

 

 

I looked for old threads about this problem, it appears that the hardboard is misconfigured. I followed the settings at

 

http://docs.blackfin.uclinux.org/doku.php?id=hw:boards:bf561-ezkit, but it doesn't give clear indication.

 

my switch settings are:

 

main board:

Switch     Setting

P1     Open

SW2     OFF,OFF,OFF,OFF,OFF,ON

SW3     ON,ON,ON,OFF

SW4     ON,ON,ON,ON,OFF,OFF

SW5     OFF,ON,ON,ON

 

USB-LAN board:

Switch     Setting

R54     Populate with 0-Ohm resistor

SW1     ON,ON,ON,OFF

SW2     OFF,OFF,OFF,OFF

JP1     Open

JP2     Closed

JP3     Open

 

Any ideas?

 

Thanks!

QuoteReplyEditDelete

 

 

2010-10-12 22:35:33     Re: SMC91111: PHY auto-negotiate timed out

Mike Frysinger (UNITED STATES)

Message: 94448   

 

please read the documentation for the addon card as linked from the bf561-ezkit page:

http://docs.blackfin.uclinux.org/doku.php?id=hw:cards:usb-lan_ez-extender

QuoteReplyEditDelete

 

 

2010-10-13 03:35:00     Re: SMC91111: PHY auto-negotiate timed out

Rui Guo (CHINA)

Message: 94460   

 

please read the documentation for the addon card as linked from the bf561-ezkit page:

http://docs.blackfin.uclinux.org/doku.php?id=hw:cards:usb-lan_ez-extender

 

---

 

But the problem occured in u-boot, but not linux. The link you provide is about linux. It's not helpful.

 

There are some links about u-boot?

 

Thanks.

QuoteReplyEditDelete

 

 

2010-10-13 09:55:40     Re: SMC91111: PHY auto-negotiate timed out

Mike Frysinger (UNITED STATES)

Message: 94474   

 

it covers the hardware revs which you have not stated

 

you also need to be using at least the latest release of u-boot which you also have not shown

Attachments

    Outcomes