2010-07-15 03:34:50     board briked after "saveenv"

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

2010-07-15 03:34:50     board briked after "saveenv"

Julien Vermillard (FRANCE)

Message: 91283   

 

Hi,

 

On a board designed after the BF537 stamp, I manage to flash & boot u-boot from NOR, but each time I change my env variables  and I save them ("saveenv") the board isn't booting anymore.

 

The u-boot I use works perfectly on my BF537-STAMP eval board.

 

Any idea ?

QuoteReplyEditDelete

 

 

2010-07-15 03:42:23     Re: board briked after "saveenv"

Julien Vermillard (FRANCE)

Message: 91284   

 

My u-boot version :

 

 

U-Boot 2008.10 (ADI-2009R1.1-rc1) (Mar 16 2010 - 09:57:53)

 

CPU:   ADSP bf537-0.2 (Detected Rev: 0.3) (bypass boot)

Board: ADI BF537 stamp board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 500 MHz, Core: 500 MHz, System: 125 MHz

RAM:   64 MB

Flash:  4 MB

In:    serial

Out:   serial

Err:   serial

Net:   Blackfin EMAC

MAC:   00:E0:22:FE:60:34

QuoteReplyEditDelete

 

 

2010-07-15 06:39:48     Re: board briked after "saveenv"

Julien Vermillard (FRANCE)

Message: 91293   

 

using the fw_* utilities works fine, apparently the problem is only using u-boot saveenv

QuoteReplyEditDelete

 

 

2010-07-15 09:29:37     Re: board briked after "saveenv"

Mike Frysinger (UNITED STATES)

Message: 91299   

 

if you dont have the same flash layout as the stamp, then you cannot use the same settings or things like this will occur

 

verify your env sector settings match your flash in your board config

 

also, you seem to be simply modifying the bf537-stamp board code.  dont do that.  create your own board files.

Attachments

    Outcomes