2010-07-03 23:34:18     bf518f-ezbrd booting kernel from NOR FLASH, Bad Data CRC

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

2010-07-03 23:34:18     bf518f-ezbrd booting kernel from NOR FLASH, Bad Data CRC

weixin zhan (CHINA)

Message: 90871   

 

bfin> bootm 0x20000000

## Booting kernel from Legacy Image at 20000000 ...

   Image Name:   Linux-2.6.28.10-ADI-2009R1.1

   Created:      2010-06-17   5:16:17 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    3811435 Bytes =  3.6 MB

   Load Address: 00001000

   Entry Point:  00190b80

   Verifying Checksum ... Bad Data CRC

ERROR: can't get kernel image!

 

 

 

 

 

 

 

bfin> printenv            

bootargs=root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,9600       

i2c     - I2C sub-system                      

icache  - enable or

console=ttyBF0,9600cache            

bootcmd=run ramboot         

iminfo

gatewayip=192.168.0.1

netmask=255.255.255.0

hostname=bf518f-ezbrd

loadaddr=0x1000000

ubootfile=u-boot.ldr

update=tftp $(loadaddr) $(ubootfile);protect off 0x20000000 0x2003FFFF;erase 0x2

0000000 0x2003FFFF;cp.b $(loadaddr) 0x20000000 $(filesize)

addip=set bootargs $(bootargs) ip=$(ipaddr):$(serverip):$(gatewayip):$(netmask):

$(hostname):eth0:off

ramargs=set bootargs root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial

,uart0,9600 console=ttyBF0,9600

ramboot=tftp $(loadaddr) uImage;run ramargs;run addip;bootm

nfsargs=set bootargs root=/dev/nfs rw nfsroot=$(serverip):$(rootpath),tcp,nfsver

s=3

nfsboot=tftp $(loadaddr) vmImage;run nfsargs;run addip;bootm

flashboot=bootm 0x20100000

stdin=serial

stdout=serial

stderr=serial

ethact=Blackfin EMAC

ethaddr=26:0C:EA:B3:80:DC

 

Environment size: 1006/8188 bytes

TranslateQuoteReplyEditDelete

 

 

2010-07-04 01:38:05     Re: bf518f-ezbrd booting kernel from NOR FLASH, Bad Data CRC

Mike Frysinger (UNITED STATES)

Message: 90872   

 

you cannot use the 4th async bank by default due to conflicts with SPI

Attachments

    Outcomes