2010-06-08 09:36:31     Failed to initialize SPI flash

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

2010-06-08 09:36:31     Failed to initialize SPI flash

Shivakumar ammanna (INDIA)

Message: 90194   

 

Hello,

 

I'm running with the latest uboot.bin (U-Boot 2010.03-svn2311 (ADI-2010R1-pre) (Jun 08 2010 - 16:11:52)) on BF537-stamp board.

 

I get following error when i try to probe serial nor flash.

 

bfin> sf probe 2

 

SF: Unsupported manufacturer FF

Failed to initialize SPI flash at 0:2

 

Daa board info: v2.0 DD2306( 25p32xx flash chip).

 

 

 

what could be the reason of this behaviour ?

 

 

 

Regards,

 

Shivakumar

QuoteReplyEditDelete

 

 

2010-06-08 14:27:07     Re: Failed to initialize SPI flash

Mike Frysinger (UNITED STATES)

Message: 90195   

 

you have to use the GPIO # now, not the SPI SSEL #

Attachments

    Outcomes