2010-04-14 01:56:43     can't get the DM9000 ID in IP04

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

2010-04-14 01:56:43     can't get the DM9000 ID in IP04

Zhi Qiang Zhang (CHINA)

Message: 88398   

 

I checkout the u-boot(svn 2244), but it can't properly read the DM9000 ID, the correct DM9000 ID is 0x90000A46, but it is 0x000a4690 by using the u-boot(svn-2244), it seems the align problem. The ID can be correctly read by using u-boot-1.1.6.

 

Regards,

 

ZhangZQ

QuoteReplyEditDelete

 

 

2010-04-14 02:01:13     Re: can't get the DM9000 ID in IP04

Mike Frysinger (UNITED STATES)

Message: 88399   

 

you can try this patch:

http://thread.gmane.org/gmane.linux.hardware.blackfin.u-boot.devel/259/focus=266

QuoteReplyEditDelete

 

 

2010-04-14 02:36:32     Re: can't get the DM9000 ID in IP04

Zhi Qiang Zhang (CHINA)

Message: 88400   

 

Yes, it works. Thank you very much!

 

 

 

Regards,

 

ZhangZQ

Attachments

    Outcomes