2010-03-26 20:20:29     Could u-boot be used for run dxe or ldr files(gnerated by visualdsp)

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

2010-03-26 20:20:29     Could u-boot be used for run dxe or ldr files(gnerated by visualdsp)

Jianxi Fu (UNITED STATES)

Message: 87743   

 

Hi

 

Could u-boot be used for run dxe or ldr files(gnerated by visualdsp)?

 

There are two VisualDSP++5.0 project. There are the same.

 

I want to use one for normally use and update, the other is used for backup.

 

So I want to put them in different locations in flash.

 

And if first one is crash, I can start the buckup.

 

Could u-boot be used for run dxe or ldr files(gnerated by visualdsp)?

 

Information:

 

BF537-stamp

VisualDSP++5 up4

 

 

Sincerely

 

Jianxi

QuoteReplyEditDelete

 

 

2010-03-27 00:25:01     Re: Could u-boot be used for run dxe or ldr files(gnerated by visualdsp)

Mike Frysinger (UNITED STATES)

Message: 87745   

 

DXE's are simply ELFs, so they probably work.  u-boot should support LDR files fine assuming you dont go reprogramming the memory controller and/or clocks.

Attachments

    Outcomes