2010-02-10 12:19:38     BF533 stamp card, U Boot 1.1.3 kernal verion lan question.

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

2010-02-10 12:19:38     BF533 stamp card, U Boot 1.1.3 kernal verion lan question.

John Crossett (UNITED STATES)

Message: 85922   

 

CPU:   ADSP BF533 Rev.: 0.3                                                   

Board: ADI BF533 Stamp board                                                  

       Support: http://blackfin.uclinux.org/                                  

       Richard Klingler <richard@uclinux.net>                                 

Clock: VCO: 497 MHz, Core: 497 MHz, System: 99 MHz                            

SDRAM: 128 MB                                                                 

FLASH:   4 MB                                                                 

In:    serial                                                                 

Out:   serial                                                                 

Err:   serial                                                                 

Net:   SMC91111 at 0x20300300                                                 

I2C:   ready                                                                  

Hit any key to stop autoboot:  0                                              

stamp>b

 

 

After having sucesfully installed a pre-built kernel to this board last week using tftpboot etc, I am now having trouble

 

getting the board at the stamp<monitor> level to recognize the lan.  This is interesting because when I boot into the

 

existing linux kernel all network operations work as they should.  At any rate,

 

stamp>set ipadd 192.168.2.20                                                  

stamp>set serverip 192.168.2.171                                              

stamp>ping 192.168.2.171                                                      

Using MAC Address 00:E0:22:FE:04:F2                                           

ping failed; host 192.168.2.171 is not alive                                  

stamp>

 

 

So. if i boot into the kernel this all works fine.

 

 

 

stamp>boot                                                                    

## Booting image at 20040000 ...                                              

   Image Name:   uClinux Kernel Image                                         

   Created:      2005-05-16   6:52:19 UTC                                     

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)                

   Data Size:    1347524 Bytes =  1.3 MB                                      

   Load Address: 00001000                                                     

   Entry Point:  00001000                                                     

   Verifying Checksum ... OK                                                  

   Uncompressing Kernel Image ... OK                                          

Starting Kernel at = 1000                                                     

Linux version 2.6.8.1 (root@sevens) (gcc version 3.4.1) #3 Mon May 16 13:05:00 5

Blackfin support (C) 2004 Analog Devices, Inc.                                

ADSP-BF533 Rev. 0.3                                                           

uClinux/BF533                                                                 

Blackfin uClinux support by blackfin.uclinux.org                              

Processor Speed: 497 MHz core clock and 99 Mhz System Clock                   

Board Memory: 128MB                                                           

Memory map:                                                                   

  text = 0x001000-0x0b98a4                                                    

  data = 0x0c3304-0x0e18c0                                                    

  bss  = 0x0e18c0-0x0f0390                                                    

  rootfs = 0x0f0390-0x4d9000                                                  

  stack = 0x0c4000-0x0c6000                                                   

Command line: 'root=/dev/mtdblock0 rw'                                        

Instruction Cache Enabled                                                     

Data Cache Enabled                                                            

Built 1 zonelists                                                             

Kernel command line: root=/dev/mtdblock0 rw                                   

Configuring Blackfin Priority Driven Interrupts                               

PID hash table entries: 16 (order 4: 128 bytes)                               

Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)               

Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)                 

Physical pages: 8000                                                          

Memory available: 124704k/130291k RAM, (36k init code, 738k kernel code, 180k d)

Blackfin Scratchpad data SRAM: 4 KB                                           

Blackfin DATA_A SRAM: 16 KB                                                   

Calibrating delay loop... 78.43 BogoMIPS                                      

Security Scaffold v1.0.0 initialized                                          

Capability LSM initialized                                                    

Mount-cache hash table entries: 512 (order: 0, 4096 bytes)                    

NET: Registered protocol family 16                                            

Blackfin DMA Controller for BF533                                             

stamp_init register the device resource to system.                            

Real Time Clock Driver v1.10e                                                 

blackfin_dpmc_init                                                            

Dynamic Power Management Controller: major=10, minor = 254                    

DPMC Driver v0.1                                                              

BlackFin BF533 serial driver version 2.00 With DMA Support                    

ttyS0 at irq = 21 is a builtin BlackFin BF533 UART                            

Enabling Serial UART Interrupts                                               

RAMDISK driver initialized: 16 RAM disks of 4096K size 1024 blocksize         

EBIU Asynchronous memory setup.                                               

smc91x.c: v1.0, mar 07 2003 by Nicolas Pitre <nico@cam.org>                   

EZ-LAN interrupt setup.                                                       

eth0: SMC91C11xFD (rev 1) at 0x20300300 IRQ 27 [nowait]                       

eth0: Ethernet addr: 00:e0:22:fe:04:f2                                        

Using cfq io scheduler                                                        

uclinux[mtd]: RAM probe address=0xf0390 size=0x3e8000                         

Creating 1 MTD partitions on "RAM":                                           

0x00000000-0x003e8000 : "EXT2fs"                                              

uclinux[mtd]: set EXT2fs to be root filesystem                                

NET: Registered protocol family 2                                             

IP: routing cache hash table of 1024 buckets, 8Kbytes                         

TCP: Hash tables configured (established 8192 bind 16384)                     

NET: Registered protocol family 1                                             

NET: Registered protocol family 17                                            

VFS: Mounted root (ext2 filesystem).                                          

Freeing unused kernel memory: 36k freed (0xba000 - 0xc2000)                   

Allocated address in l1sram_alloc is 4286578688                               

bf533_change_speed: baud = 57600, cval = 0x13                                 

                                                                              

Welcome to:                                                                   

       ____ _  _                                                              

      /  __| ||_|             _  _                                            

_   _| |  | | _ ____  _   _ \ \/ /                                           

| | | | |  | || |  _ \| | | | \  /                                            

| |_| | |__| || | | | | |_| | /  \                                            

|  ___\____|_||_|_| |_|\____|/_/\_\                                           

|_|                        e                                                  

                                                                              

For further information see:                                                  

http://www.uclinux.org/                                                       

http://blackfin.uclinux.org/                                                  

                                                                              

th0: link down                                                                

root:~> ieth0: link up, 100Mbps, full-duplex, lpa 0x45E1                      

                                                                              

 

root:~> ifconfig eth0 192.168.2.20                                            

root:~> ping 192.168.2.171                                                    

PING 192.168.2.171 (192.168.2.171): 56 data bytes                             

64 bytes from 192.168.2.171: icmp_seq=0 ttl=64 time=36.6 ms                   

64 bytes from 192.168.2.171: icmp_seq=1 ttl=64 time=1.7 ms                    

64 bytes from 192.168.2.171: icmp_seq=2 ttl=64 time=1.7 ms                    

64 bytes from 192.168.2.171: icmp_seq=3 ttl=64 time=2.0 ms                    

64 bytes from 192.168.2.171: icmp_seq=4 ttl=64 time=73.7 ms                   

64 bytes from 192.168.2.171: icmp_seq=5 ttl=64 time=1.9 ms                    

^C64 bytes from 192.168.2.171: icmp_seq=6 ttl=64 time=1.7 ms                  

64 bytes from 192.168.2.171: icmp_seq=7 ttl=64 time=1.7 ms                    

64 bytes from 192.168.2.171: icmp_seq=8 ttl=64 time=1.7 ms                    

^V^X64 bytes from 192.168.2.171: icmp_seq=9 ttl=64 time=2.1 ms                

64 bytes from 192.168.2.171: icmp_seq=10 ttl=64 time=1.7 ms     

 

 

 

So.. I would respectifllly ask anyone that reads this and might know the answer to give me a buzz on this

 

jrcrossett@ieee.org

 

 

 

thanks.

QuoteReplyEditDelete

 

 

2010-02-10 15:06:16     Re: BF533 stamp card, U Boot 1.1.3 kernal verion lan question.

Robin Getz (UNITED STATES)

Message: 85926   

 

John:

 

We fixed alot of things - that require an upgrade of U-Boot, and the kernel.

 

Did you boot a new kernel, with an old U-Boot?

 

-Robin

Attachments

    Outcomes