2010-01-19 02:02:02     u-boot and BF527 USB OTG problem

Document created by Aaronwu Employee on Sep 25, 2013
Version 1Show Document
  • View in full screen mode

2010-01-19 02:02:02     u-boot and BF527 USB OTG problem

Anoop sasi (INDIA)

Message: 84728   

 

Hi all,

 

Am using BF527 as my dovelopment kit and i have used u-boot-2008.10-2009R1-rc3 as my boot loader . BF527 has only one USB OTG support but I need to connect Multiple USB devices(USB Keyboard, mouse and MSD) at a time, as a solution i tried using USB 2.0 4 port hub. Then i tried to detect the usb device using usb start command it detected the usb device but could not detect it as a mass storage device. what might be the problem. plaese help me.

 

Boot loader configurations made for USB  upport

 

/*

* USB Setting

*/

#if !defined(__ADSPBF522__) && !defined(__ADSPBF523__)

#define CONFIG_USB

#define CONFIG_MUSB_HCD

#define CONFIG_USB_BLACKFIN

#define CONFIG_USB_STORAGE

#define CONFIG_MUSB_TIMEOUT 100000

#endif

 

 

This is the error log

 

bfin> usb start

(Re)start USB...

USB:   scanning bus for devices...

      USB device not accepting new address (error=2)

3 USB Device(s) found

       scanning bus for storage devices... 0 Storage Device(s) found

 

 

bfin> usb tree

 

Device Tree:

  1  Hub (12MBit/s, 0mA)

  |   MUSB Root Hub

  |

  +-2  Hub (480MBit/s, 100mA)

    |

    +-3  See Interface (480MBit/s, 0mA)

     

bfin>

QuoteReplyEditDelete

 

 

2010-01-19 02:06:06     Re: u-boot and BF527 USB OTG problem

Mike Frysinger (UNITED STATES)

Message: 84729   

 

your colleague has already posted this question and been given the answer:

http://blackfin.uclinux.org/gf/forummessage/84711

Attachments

    Outcomes