2009-11-20 02:57:31     USB Driver & MSC class Support in UBOOT

Document created by Aaronwu Employee on Sep 24, 2013
Version 1Show Document
  • View in full screen mode

2009-11-20 02:57:31     USB Driver & MSC class Support in UBOOT

Sada M (INDIA)

Message: 82552   

 

Hi ,

 

Do we have USB Driver & MSC Class support in UBOOT ?

 

We would like use USB in UBOOT for application booting once the uboot is booted from flash.

 

Thanks & Regards,

 

Sada.

QuoteReplyEditDelete

 

 

2009-11-20 10:49:14     Re: USB Driver & MSC class Support in UBOOT

Robin Getz (UNITED STATES)

Message: 82599   

 

Sada:

 

Yes - there is USB support in U-Boot.

 

See:

 

https://docs.blackfin.uclinux.org/doku.php?id=bootloaders:u-boot:usb

 

(which I'm in the process of writing - so if it is empty - come back in 5 minutes).

QuoteReplyEditDelete

 

 

2009-11-23 02:04:21     Re: USB Driver & MSC class Support in UBOOT

Sada M (INDIA)

Message: 82631   

 

Hi Robin,

 

Sorry, I could not open the link provided by you ( hope it is still under construction ).

 

Could you please let us know once it is done ?

 

Also, we hope that with this USB support we should be able to read a file from the USB Stick / USB HDD.                                In that case i hope USB MSC Class driver & FAT 32 will be available in UBOOT. Please confirm.

 

Thanks & Regards,

 

Sada.

QuoteReplyEditDelete

 

 

2009-11-23 06:49:38     Re: USB Driver & MSC class Support in UBOOT

Robin Getz (UNITED STATES)

Message: 82641   

 

Sada:

 

There is a difference between the link not working, and the docs site being down.

 

It is done - as soon as the docs machine is repaired, it will be there.

 

As far as confirmation - read the documentation.

 

-Robin

Attachments

    Outcomes