2009-11-12 06:06:06     Does U-Boot will work on BF533-EZKIT Rev 1.3?

Document created by Aaronwu Employee on Sep 24, 2013
Version 1Show Document
  • View in full screen mode

2009-11-12 06:06:06     Does U-Boot will work on BF533-EZKIT Rev 1.3?

Vladimir Klochkov (RUSSIAN FEDERATION)

Message: 82311   

 

I have old version BF533-EZKIT Rev 1.3, Silicon revision 0.2.

I read of course https://docs.blackfin.uclinux.org/doku.php?id=hw:boards:bf533-ezkit.

Is it true that u-boot will not work on my board?

QuoteReplyEditDelete

 

 

2009-11-12 11:08:31     Re: Does U-Boot will work on BF533-EZKIT Rev 1.3?

Robin Getz (UNITED STATES)

Message: 82324   

 

Vladimir:

 

Have a look at:

 

https://docs.blackfin.uclinux.org/doku.php?id=uclinux-dist:features

 

Versions are the same in U-Boot as in the uClinux-dist.

QuoteReplyEditDelete

 

 

2009-11-13 01:46:35     Re: Does U-Boot will work on BF533-EZKIT Rev 1.3?

Vladimir Klochkov (RUSSIAN FEDERATION)

Message: 82340   

 

Robin:

 

Thank You for help!

 

I am newbie here. And I read info sequentionaly. May be usefull place reference to this page in "Introduction".

QuoteReplyEditDelete

 

 

2009-11-13 07:57:37     Re: Does U-Boot will work on BF533-EZKIT Rev 1.3?

Vladimir Klochkov (RUSSIAN FEDERATION)

Message: 82356   

 

Hello, Robin.

 

I get away BF533-EZKIT Rev 1.3.

 

I try again with BF548-EZKIT Rev1.3. Silicon revision 0.0.

 

Compile U-Boot for bf548-ezkit_config - ok.

Program u-boot by VisualDSP - ok.

Reset and read on terminal :

 

===========================================

U-Boot 2008.10 (ADI-2009R1-rc3) (Nov 12 2009 07:35:34)

 

 

CPU: ADSP bf548-0.0 (Detected Rev: 0.0) (parallel flash boot)

.... etc

============================================

 

I read second string and become happy.

 

But I return to You previous post and understand:

 

1) bf548-0.0 not in list  https://docs.blackfin.uclinux.org/doku.php?id=uclinux-dist:features,

2) but "Versions are the same in U-Boot as in the uClinux-dist"

3) and U-Boot expected bf548-0.0.

 

Can I try to work with this board? uImage  write "Kernel panic - not syncing ..." Can I recompile kernel from sources for this silicon revision or I will have only trouble?

QuoteReplyEditDelete

 

 

2009-11-13 10:09:25     Re: Does U-Boot will work on BF533-EZKIT Rev 1.3?

Robin Getz (UNITED STATES)

Message: 82360   

 

Vladimir:

 

BF548 DDR is not stable on 0.1 - due to anomaly 05000448. There were so few B F548-0.0 silicon shipped anywhere, we stopped testing on it.

 

-Robin

QuoteReplyEditDelete

 

 

2009-11-13 10:11:04     Re: Does U-Boot will work on BF533-EZKIT Rev 1.3?

Mike Frysinger (UNITED STATES)

Message: 82361   

 

just because it works doesnt mean it's supported

Attachments

    Outcomes