2009-08-27 04:15:43     u-boot network program

Document created by Aaronwu Employee on Sep 24, 2013
Version 1Show Document
  • View in full screen mode

2009-08-27 04:15:43     u-boot network program

jun jia (CHINA)

Message: 79273   

 

hi,everyone

 

    I'v met a program about u-boot network,the tftp can't work,I mean is tftp always timeout. the u-boot I use is u-boot-1.1.6-2008r1.5.  

 

    In my custom we have SMSC9215 chip is interfaced to BF548 with the AMS1 bank. the hardware circuit as bf548-ezkit.

 

    when i directly use u-boot for bf548-ezkit , then u-boot says"can't detect  Lan9x18".  therefore I just add ID_REV of smsc9215i to smsc9118.h and smsc9118.c. u-boot can detect the net chip. buf tftp can't work.

 

     the driver for smsc9218i coud not work with smsc9215i?

 

    Am i missing  anything?

TranslateQuoteReplyEditDelete

 

 

2009-08-27 04:38:56     Re: u-boot network program

Mike Frysinger (UNITED STATES)

Message: 79275   

 

we've only tested the part that is on the bf548-ezkit.  hacking up an old driver isnt going to work.  get the 2009R1 release which has an updated SMSC driver.

QuoteReplyEditDelete

 

 

2009-08-27 07:51:25     Re: u-boot network program

jun jia (CHINA)

Message: 79280   

 

Hi , Mike

 

    I'v get the 2009r1 release source. I directly compile u-boot , and the put it on My board. this time u-boot can detect my net  chip(i don't modify the u-boot code). but whe I use tftp to get file , u-boot stay on "loading *" , the u-boot display infomation is :

 

bfin> tftp 1000000 u-boot.ldr

smc911x: initializing

smc911x: detected LAN9215 controller

smc911x: phy initialized

smc911x: MAC 00:e0:22:fe:b7:8a

TFTP from server 192.168.231.22; our IP address is 192.168.231.28

Filename 'u-boot.ldr'.

Load address: 0x1000000

Loading: *

TranslateQuoteReplyEditDelete

 

 

2009-08-27 08:03:57     Re: u-boot network program

Mike Frysinger (UNITED STATES)

Message: 79281   

 

are you sure the tftp server is enabled and working ?

 

otherwise, use wireshark to make sure packets are going out and try enabling debugging in the driver.  and make sure you're using 16bit mode.

 

if you still have problems with the driver, you should ask the guy who wrote it.  it wasnt us -- read the source to find out.

QuoteReplyEditDelete

 

 

2009-08-28 01:20:01     Re: u-boot network program

jun jia (CHINA)

Message: 79338   

 

Mike , thanks.

 

    The program of network is solved. the reason that cause tftp doesn't works well maybe is the operation timming between blackfin and smsc9215i . I channge the value of EBIU_AMBCTL0  to FFC27BB0 , then the tftp works well.

TranslateQuoteReplyEditDelete

Attachments

    Outcomes