2009-08-06 07:28:21     who successfully used dm9000e in u-boot?

Document created by Aaronwu Employee on Sep 24, 2013
Version 1Show Document
  • View in full screen mode

2009-08-06 07:28:21     who successfully used dm9000e in u-boot?

xm ye (CHINA)

Message: 78419   

 

hi,all

 

i used u-boot-1.1.6, my ehercard is dm9000e,with no EEPROM, my config like this

 

#define ADI_CMDS_NETWORK      1

#define CONFIG_DRIVER_ETHER     1

#define CONFIG_DRIVER_DM9000    1

 

//#undef  CONFIG_DM9000_HAVE_EEPROM      

#define CONFIG_ETHADDR    02:80:ad:20:31:e8

 

 

and i chang some code  in dm9000.c,it can read VID&PID,so in the physical it is no wrong,now

 

but it can\'t ping or tftp.  I used tcpdump to detect the net ,it was data streams (like arp,i really not understand ^ ^)in the line.so i want to  know if   the physically read write still some wrong or the U-BOOT net  fuction does\'nt match with dm9000e. thank you very much !

QuoteReplyEditDelete

 

 

2009-08-07 02:38:49     Re: who successfully used dm9000e in u-boot?

xm ye (CHINA)

Message: 78477   

 

ok ,i have solved it.

 

i add some "asm(ssync)" in read write function.

Attachments

    Outcomes