2009-07-01 06:39:01     ADSP-BF518F EZ-Borad u-boot network cannot work

Document created by Aaronwu Employee on Sep 24, 2013
Version 1Show Document
  • View in full screen mode

2009-07-01 06:39:01     ADSP-BF518F EZ-Borad u-boot network cannot work

Bill Xie (CHINA)

Message: 76588   

 

Hi,Sir

 

      I use ADSP-BF518F EZ-Borad Rev 0.2, the network canot work. the output mesage is:

 

 

 

U-Boot 2008.10-00143-g46bf1eb-dirty (ADI-2009R1-pre) (Nov 20 2008 - 21:55:38)

 

CPU:   ADSP bf518-0.0 (Detected Rev: 0.0)

Board: ADI BF518F EZ-Board board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 400 MHz, Core: 400 MHz, System: 80 MHz

RAM:   64 MB

Flash:  4 MB

In:    serial

Out:   serial

Err:   serial

Net:   Blackfin EMAC

MAC:   F2:8F:87:22:20:12

Hit any key to stop autoboot:  0

 

 

 

bfin> print

 

hostname=bf518f-ezbrd

loadaddr=0x1000000

ubootfile=u-boot.ldr

update=tftp $(loadaddr) $(ubootfile);eeprom write $(loadaddr) 0x0 $(filesize)

addip=set bootargs $(bootargs) ip=$(ipaddr):$(serverip):$(gatewayip):$(netmask):

$(hostname):eth0:off

ramargs=set bootargs root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600 conso

le=ttyBF0,57600

ramboot=tftp $(loadaddr) uImage;run ramargs;run addip;bootm

nfsargs=set bootargs root=/dev/nfs rw nfsroot=$(serverip):$(rootpath),tcp,nfsver

s=3

nfsboot=tftp $(loadaddr) vmImage;run nfsargs;run addip;bootm

flashboot=bootm 0x20100000

ethact=Blackfin EMAC

ethaddr=F2:8F:87:22:20:12

serverip=192.168.0.204

baudrate=115200

ipaddr=192.168.0.209

stdin=serial

stdout=serial

stderr=serial

 

Environment size: 918/8188 bytes

 

.bfin> ping 192.168.0.204

Using Blackfin EMAC device

ping failed; host 192.168.0.204 is not alive

 

Does the network driver have problem? Please  help me to solve this question,thanks!

 

--Bill

QuoteReplyEditDelete

 

 

2009-07-01 08:41:32     Re: ADSP-BF518F EZ-Borad u-boot network cannot work

Robin Getz (UNITED STATES)

Message: 76592   

 

Bill:

 

Just to start with the basics:

 

- your network cable is plugged in

 

- the host at 192.168.0.204 is alive and responds to pings (sometimes firewal software turns this off).

 

-Robin

QuoteReplyEditDelete

 

 

2009-07-01 09:32:05     Re: ADSP-BF518F EZ-Borad u-boot network cannot work

Mike Frysinger (UNITED STATES)

Message: 76596   

 

install the latest 2009R1 u-boot from our site.  that version probably doesnt have the updates to deal with the changes made to the latest board.

QuoteReplyEditDelete

 

 

2009-07-01 21:22:34     Re: ADSP-BF518F EZ-Borad u-boot network cannot work

Bill Xie (CHINA)

Message: 76609   

 

Robin,

 

     Thank you for your reply,the cable is ok and plugged in .host IP is also alive and it is ok by other PC to ping.

 

 

 

-Bill

QuoteReplyEditDelete

 

 

2009-07-01 21:40:58     Re: ADSP-BF518F EZ-Borad u-boot network cannot work

Bill Xie (CHINA)

Message: 76611   

 

Mike,

 

   Thank you for  your reply. I downloaded  the latest u-boot.when make bf518f-ezbrd_config,the command line is not return .I try install latest toolchain.

 

 

 

--Bill

QuoteReplyEditDelete

 

 

2009-07-01 21:44:15     Re: ADSP-BF518F EZ-Borad u-boot network cannot work

Mike Frysinger (UNITED STATES)

Message: 76612   

 

i said download the 2009R1-rc2 binary.  there is no need for you to build it yourself.

QuoteReplyEditDelete

 

 

2009-07-01 22:38:07     Re: ADSP-BF518F EZ-Borad u-boot network cannot work

Bill Xie (CHINA)

Message: 76613   

 

Mike,

 

    Thank you,I just  use u-boot-bf518f-ezbrd-spi.ldr from http://blackfin.uclinux.org/gf/project/u-boot/frs/ ,the network is not ok.

 

Which link to download  2009R1-rc2?

 

 

 

-Bill

QuoteReplyEditDelete

 

 

2009-07-01 22:41:32     Re: ADSP-BF518F EZ-Borad u-boot network cannot work

Mike Frysinger (UNITED STATES)

Message: 76614   

 

click the u-boot link on the frs page to view all releases

QuoteReplyEditDelete

 

 

2009-07-01 23:13:58     Re: ADSP-BF518F EZ-Borad u-boot network cannot work

Bill Xie (CHINA)

Message: 76615   

 

Mike,

 

    Thank you.I found the file.It is ok for network.

 

-Bill

Attachments

    Outcomes