FAQ: Can I use MATLAB/Simulink with the ADSP-CM40x?

Document created by CraigG on Sep 24, 2013Last modified by CraigG on Sep 24, 2013
Version 2Show Document
  • View in full screen mode

Question

Can I use MATLAB and Simulink with the ADSP-CM40x and IAR Tool-chain?

 

==============================

 

Answer

While there is no direct interface between the IAR Tool-chain and MATLAB or Simulink, Mathworks offer the “Embedded Coder” product, an add-on which can generate portable C/C++ code from a MATLAB algorithm or Simulink model. The code generated from Embedded Coder can be compiled for the ADSP-CM40x processor using the IAR Tool-chain.

 

Embedded Coder further supports ARM by generating code that is optimized for ARM Cortex-M processors, such as the ADSP-CM40x. This ARM optimized code offers up to a significant execution performance improvement over ANSI/ISO C and supports MATLAB code, Simulink blocks, and DSP System Toolbox filters.

 

For more information, visit the Embedded Coder Product Page on the Mathworks website.

Attachments

    Outcomes