2009-05-30 22:34:25     Exception with u-boot.1.1.5-bf1

Document created by Aaronwu Employee on Sep 18, 2013
Version 1Show Document
  • View in full screen mode

2009-05-30 22:34:25     Exception with u-boot.1.1.5-bf1

roy xue (CHINA)

Message: 74827   

 

Hi, all

 

I'm using u-boot.1.1.5-bf1. I want the board boot silently, so I add #define CONFIG_SILENT_CONSOLE at configure files.

 

I used go command to test the new uboot , it can use but have a "Exception!" error. when write the uboot to the flash, the

 

board can't boot up.

 

Definded the CONFIG_CMDLINE_EDITING also have that problem.

 

Any  advance would be appreciate.

 

-----------------------Here is the uboot out put:----------------------------------

 

ip04>tftp 0x1000000 u-boot.bin

ip04>go 0x1000000

## Starting application at 0x01000000 ...

Exception!

U-Boot 1.1.5 (May 31 2009 - 10:01:31)

 

CPU:   ADSP BF532 Rev.: 0.3

Board: IP04 IP-PBX

       http://www.rowetel.com/ucasterisk/ip04.html

Clock: VCO: 400 MHz, Core: 400 MHz, System: 133 MHz

SDRAM: 64 MB

In:    serial

Out:   serial

Err:   serial

256 MiB

DM9000#0

starting from spi flash

Hit any key to stop autoboot:  0

ip04>

 

----------------------------end-------------------------------------------

 

Roy

QuoteReplyEditDelete

 

 

2009-05-30 23:40:33     Re: Exception with u-boot.1.1.5-bf1

Mike Frysinger (UNITED STATES)

Message: 74828   

 

that version of u-boot was not done by us.  use a supported version or ask on the asterisk forums.

QuoteReplyEditDelete

Attachments

    Outcomes