2008-10-24 06:30:50     usb commands on u-boot for bf527-ez-kit

Document created by Aaronwu Employee on Sep 18, 2013
Version 1Show Document
  • View in full screen mode

2008-10-24 06:30:50     usb commands on u-boot for bf527-ez-kit

abhrajit datta (INDIA)

Message: 64156   

 

Hi,

 

i want to use the usb commands in u-boot for bf-527 EZ-kit. As they are not set by default i manually added them in include/configs/bfin_adi_common.h. But when i compile i get errors such as :

 

part.c:274:3: error: #error neither CONFIG_MAC_PARTITION nor CONFIG_DOS_PARTITION nor CONFIG_ISO_PARTITION configured!

 

 

As i am new to u-boot i don't know where to configure the mac partition etc, or do we need to configure it for using the usb-commands. Please help me to configure the usb commands in u-boot.

 

Thanks ,

 

abhri

QuoteReplyEditDelete

 

 

2008-10-24 08:10:20     Re: usb commands on u-boot for bf527-ez-kit

Robin Getz (UNITED STATES)

Message: 64161   

 

Abhri:

 

USB is not something that is supported on USB yet (sorry) - we are working on it, and plan to have it done in the next few months (sometime before the end of the year).

 

-Robin

Attachments

    Outcomes