2008-09-27 05:58:38     Uboot for BF531

Document created by Aaronwu Employee on Sep 18, 2013
Version 1Show Document
  • View in full screen mode

2008-09-27 05:58:38     Uboot for BF531

Benix Samuel (INDIA)

Message: 62851   

 

Can anyone give me the source code of Uboot for BF531 processor?

QuoteReplyEditDelete

 

 

2008-09-27 08:31:38     Re: Uboot for BF531

Mike Frysinger (UNITED STATES)

Message: 62854   

 

there is only "U-Boot for the Blackfin processor".  it is all the same source tree.  download it from the u-boot file release page.

 

QuoteReplyEditDelete

 

 

2008-09-27 11:42:52     Re: Uboot for BF531

Benix Samuel (INDIA)

Message: 62857   

 

HI Mike,

 

 

 

I want to configure u-boot-1.1.6-2008R1.5 for my customized board. I have 16bit STM flash. I want to make u-boot.LDR for my  flash. So what are the changes I should make in configuration files and other files. Advance thanks.

 

 

 

 

 

Benix.

 

--------------------------------------------------------------------------

 

 

 

 

QuoteReplyEditDelete

 

 

2008-09-27 12:37:33     Re: Uboot for BF531

Mike Frysinger (UNITED STATES)

Message: 62858   

 

read the documentation:

http://docs.blackfin.uclinux.org/doku.php?id=bootloaders:u-boot

Attachments

    Outcomes