2008-09-21 10:52:09     uImage.ext2 File Format

Document created by Aaronwu Employee on Sep 18, 2013
Version 1Show Document
  • View in full screen mode

2008-09-21 10:52:09     uImage.ext2 File Format

Appalayagari Sreedhar (INDIA)

Message: 62486   

 

Hi,

 

I am working on a custom board with u-boot 1.1.6 2007 R1, uClinux distribution 2007 R1-RC3.

 

I build the kernel images using the command >make

 

The uImage will be in compressed format.

 

What will be the uImage File Format, Can anyone give me the details of the uImage file format and also

 

when it unCompresses in u-boot what will the size of the compressed file.

 

Best Regards, Sreedhar.

QuoteReplyEditDelete

 

 

2008-09-21 16:07:19     Re: uImage.ext2 File Format

Mike Frysinger (UNITED STATES)

Message: 62487   

 

read the upstream u-boot documentation and the source code it ... it explains the uImage format

Attachments

    Outcomes