2008-09-05 16:29:32     U-Boot on SST SPI serial EEPROM with BF533-ezkit

Document created by Aaronwu Employee on Sep 18, 2013
Version 1Show Document
  • View in full screen mode

2008-09-05 16:29:32     U-Boot on SST SPI serial EEPROM with BF533-ezkit

Paul Leslie (CANADA)

Message: 61715   

 

Has anyone got a Uboot image for a BF533 Ezkit to load uboot from a

 

SST SPI memory device ( SST25VF016B) .

 

I am running on a windows machine and don't know Linux so I can't compile the source.

 

I am looking to download applications compiled in VDSP with Uboot.

 

Any suggestions would be appreciated,

 

cheers,

 

Paul

QuoteReplyEditDelete

 

 

2008-09-05 16:36:35     Re: U-Boot on SST SPI serial EEPROM with BF533-ezkit

Mike Frysinger (UNITED STATES)

Message: 61716   

 

the 2008R1.5 release should work with SST flashes (but we've only tested the one that is on the BF526-EZKIT board)

 

we dont provide binaries around here ... you'll have to build one yourself as the BF533-EZKIT does not enable SPI support by default -- the board's SPI header is useless and so there isnt any easy way to test things

 

if you dont want to dual boot linux, then just install colinux

QuoteReplyEditDelete

Attachments

    Outcomes