2008-08-07 06:03:44     data transfer

Document created by Aaronwu Employee on Sep 18, 2013
Version 1Show Document
  • View in full screen mode

2008-08-07 06:03:44     data transfer

Pranay Upadhyay (INDIA)

Message: 60094   

 

Hello sir,

 

    I have compiled the u-boot 2008R1, and formed the uboot binary file .After loading the u-boot, I am trying to sending the file but  data is not transmitting through the kermit in hyperterminal.The size of formed u-boot is 445 KB.Is it right.I have change only clock frequency 486 MHZ and data rate 115200 in bf-561 config.h file. Can you suggest me something about this?

 

-REGARDS

 

Pranay

 

 

 

 

QuoteReplyEditDelete

 

 

2008-08-07 15:23:00     Re: data transfer

Robin Getz (UNITED STATES)

Message: 60122   

 

Pranay:

 

What is your hardware? Custom board or an EZkit? Default U-Boot images (to at least compare sizes) are avalible in the files section.

 

-Robin

QuoteReplyEditDelete

 

 

2008-08-07 23:58:45     Re: data transfer

Pranay Upadhyay (INDIA)

Message: 60130   

 

Hello sir,

 

My hardware is the Ez-kit BF561.But in my appliaction we need different CCLK and SCLK , so I have change in it.

 

-Regards

 

Pranay

QuoteReplyEditDelete

 

 

2008-08-08 10:53:57     Re: data transfer

Mike Frysinger (UNITED STATES)

Message: 60174   

 

post the changes you have actually made to your board config file

 

then post the actual commands you are running and the errors you are seeing

Attachments

    Outcomes