2008-07-22 12:02:01     Default Load address

Document created by Aaronwu Employee on Sep 18, 2013
Version 1Show Document
  • View in full screen mode

2008-07-22 12:02:01     Default Load address

Appalayagari Sreedhar (INDIA)

Message: 59238   

 

Hi,

 

romfs size is 16MB in my project.

 

In board config file I have modified the CFG_LOAD_ADDR to 0x1200000 its properly booting.

 

do I need to modify both CONFIG_LOADADDR and CFG_LOAD_ADDR

 

or CFG_LOAD_ADDR alone works fine?

 

Can anyone explains for what this CONFIG_LOADADDR is used?

 

I have checked the u-boot documentation i could not find anything

 

Best Regards,Sreedhar

QuoteReplyEditDelete

 

 

2008-07-22 13:50:58     Re: Default Load address

Robin Getz (UNITED STATES)

Message: 59241   

 

Sreedhar:

 

Use the source - that is what it is there for.

 

try something like:

 

rgetz@imhotep:~/blackfin/trunk/u-boot/u-boot-1.1.6> grep -Rl CONFIG_LOADADDR ./* | grep -v svn

 

and then

 

rgetz@imhotep:~/blackfin/trunk/u-boot/u-boot-1.1.6> grep -Rl CONFIG_LOAD_ADDR ./* | grep -v svn

 

and have a look at the files that it comes back with.

QuoteReplyEditDelete

 

 

2008-07-22 22:04:30     Re: Default Load address

Mike Frysinger (UNITED STATES)

Message: 59252   

 

CONFIG_LOADADDR is the default value for the "loadaddr" env var while CFG_LOAD_ADDR is the default load address when the "loadaddr" env var does not exist

 

for Blackfin, we just define them to the same value

Attachments

    Outcomes