2008-04-30 06:05:03     BF533 EZKIT u-boot can not work

Document created by Aaronwu Employee on Sep 17, 2013
Version 1Show Document
  • View in full screen mode

2008-04-30 06:05:03     BF533 EZKIT u-boot can not work

maggie xu (CHINA)

Message: 55284    Hi all,

 

I have download  u-boot-exkit533.hex.gz form http://blackfin.uclinux.org/gf/project/u-boot/frs/?action=FrsReleaseBrowse&frs_package_id=67 and I decompress the file.In VDSP++ 5.0  "tools->flash programmer", I load the driver "BF533EzFlashDriver.dxe" and then in programming page I select  "Erase all", "Intel Hex" file format, press "program" buttom.When it is OK, I open HyperTerminal but there is nothing I can see.

 

BF533 EZKit LITE REV 1.6

 

SW3: 1 on, 2-6 off

SW9: 1-5 on, 6 off

SW1: all off

SW2: all off

 

HyperTerminal: 57600 8 none 1 none

 

thahks

 

 

QuoteReplyEditDelete

 

 

2008-04-30 15:43:59     Re: BF533 EZKIT u-boot can not work

Mike Frysinger (UNITED STATES)

Message: 55310    "u-boot-exkit533.hex.gz" is obviously an old release.  only use the latest release (2008R1).

QuoteReplyEditDelete

 

 

2008-04-30 20:11:07     Re: BF533 EZKIT u-boot can not work

maggie xu (CHINA)

Message: 55323   

 

Thank you.

 

I also download "u-boot-bf533-ezkit-bypass-2008R1.bin" .In VDSP++5.0 "tools->flash programmer" program page, I select "binary" and then press "program" button.When it is OK, there is nothing in HyperTerminal, too.

QuoteReplyEditDelete

 

 

2008-04-30 20:23:28     Re: BF533 EZKIT u-boot can not work

Mike Frysinger (UNITED STATES)

Message: 55324   

 

you can validate your board switch settings against the documentation:

http://docs.blackfin.uclinux.org/doku.php?id=hw:boards:bf533-ezkit

 

you can check your serial settings with this documentation:

http://docs.blackfin.uclinux.org/doku.php?id=terminal_programs&s[]=minicom

Attachments

    Outcomes