2008-04-23 13:20:08     BF533 EZKIT Flash error: Copy to Flash.....Outside available Flash

Document created by Aaronwu Employee on Sep 17, 2013
Version 1Show Document
  • View in full screen mode

2008-04-23 13:20:08     BF533 EZKIT Flash error: Copy to Flash.....Outside available Flash

hong li (CHINA)

Message: 54796    Hi everyone:

 

                   I want to burn uclinux to bf533 ezkit flash, I have burn uboot to bf533 ezkit flash successfully, Then I download uImage to the RAM, the start address is 0x01000000, the uImage's size is 1397912 bytes,and  I send command as follows:

 

ezkit>cp.b 0x01000000 0x20020000 1397912

 

then show error:

 

Copy to Flash.....Outside available Flash

 

Anyone can help me?

 

In order to slove this problem  What should i do? thanks

QuoteReplyEditDelete

 

 

2008-04-23 15:58:32     Re: BF533 EZKIT Flash error: Copy to Flash.....Outside available Flash

Robin Getz (UNITED STATES)

Message: 54801    Hong:

 

The solution is to:

-  get a different hardware platform - the 533 EZKit does not have enough flash on it.

OR

- make your image smaller. Look in the FAQs.

 

-Robin

QuoteReplyEditDelete

 

 

2008-04-23 22:41:18     Re: BF533 EZKIT Flash error: Copy to Flash.....Outside available Flash

hong li (CHINA)

Message: 54814   

 

Robin:

 

          The 533 ezkit  Flash is 2M , But my uImage is only 1.33M, the uboot is 0.3M,  I think the Flash is  enough.

 

                     There is other way to slove this problem ?

 

thanks

QuoteReplyEditDelete

 

 

2008-04-23 23:23:02     Re: BF533 EZKIT Flash error: Copy to Flash.....Outside available Flash

hong li (CHINA)

Message: 54816   

 

Robin

 

         I  slove this problem

 

         I shoule use the commond as follow:

 

          cp.b 0x01000000 0x20020000 0x00155498

 

         thanks

Attachments

    Outcomes