2008-04-20 04:59:08     u-boot for bf533-ezkit doesn't work properly~~

Document created by Aaronwu Employee on Sep 17, 2013
Version 1Show Document
  • View in full screen mode

2008-04-20 04:59:08     u-boot for bf533-ezkit doesn't work properly~~

Samuel Lin (CHINA)

Message: 54567   

 

HI all:

 

    I compile the u-boot1.1.6 for bf533-ezkit board. But it doesn't work properly....When I set the switch to 11 on the board(according to some previous thread) and change the BFIN_BOOT_BYPASS  to BFIN_BOOT_SPI_MASTER in includes/configs/bf533-ezkit.h, I can only see !a@FIN> in the terminal. It seems that initcode.c has been executed, but something was wrong after that. Anybody can help me out? Or who can give me a u-boot.ldr file which can be work on the bf533-ezkit board?

 

    BTW: My board is bf533-ezkit REV 2.1. And using VDSP++(5.0) ->Tools->Flash programmer, BF533FzFlash.DXE to write the u-boot.ldr file to the board

 

Thanks~~~~

TranslateQuoteReplyEditDelete

 

 

2008-04-20 05:15:49     Re: u-boot for bf533-ezkit doesn't work properly~~

Mike Frysinger (UNITED STATES)

Message: 54568    we dont have any addon cards for the bf533-ezkit to test booting out of spi.  we've only tested bf533-stamp and we know that it works fine.

 

assuming you've followed the debugging steps outlined in the wiki, you'll probably have to hook up jtag to find out where it's failing.

Attachments

    Outcomes