2008-04-06 23:05:09     Boot from spi flash

Document created by Aaronwu Employee on Sep 17, 2013
Version 1Show Document
  • View in full screen mode

2008-04-06 23:05:09     Boot from spi flash

DAVID ZHOU (CHINA)

Message: 53717    In my board, I want to boot  from spi flash, because thers is no parallel flash in my board.

 

I have known that how to make u-boot for spi boot, but I do not know which address of the spi flash should I put for my kernel?

 

Could any one give me some help ?

QuoteReplyEditDelete

 

 

2008-04-06 23:18:14     Re: Boot from spi flash

Mike Frysinger (UNITED STATES)

Message: 53720    what address are you talking about ?  SPI flash is not directly addressable

QuoteReplyEditDelete

 

 

2008-04-06 23:30:44     Re: Boot from spi flash

DAVID ZHOU (CHINA)

Message: 53722    I mean that : My u-boot , linux kernel and filesystem all will be stored in the spi flash, how should I config or arrange them?

QuoteReplyEditDelete

 

 

2008-04-07 00:18:04     Re: Boot from spi flash

Mike Frysinger (UNITED STATES)

Message: 53725    partition layout is completely up to you.  there is no "correct" layout.  the layout entirely reflects your needs as well as your products' needs.

QuoteReplyEditDelete

Attachments

    Outcomes