2008-03-05 14:56:09     Error while downloading svn

Document created by Aaronwu Employee on Sep 17, 2013
Version 1Show Document
  • View in full screen mode

2008-03-05 14:56:09     Error while downloading svn

Ivan Koryakovskiy (RUSSIAN FEDERATION)

Message: 52128   

 

Hello!

 

I am new to SVN and can't solve a problem myself. I am trying to download an u-boot SVN 2008. I have installed a  prgram for svn and write in command line "".

 

Process starts, but then an error occures:

 

In directory 'u-boot\u-boot-1.1.6\doc'

 

Can't move source to dest.

 

Can't move 'u-boot\u-boot-1.1.6\doc\.svn\tmp\prop-base\README.sbc8560.svn-base' to 'u-boot\u-boot-1.1.6\doc\.svn\prop-base\README.sbc8560.svn-base' File not found.

 

 

 

The same problem is with toolchain file 'toolchain\uClibc\extra\config\.svn\tmp\text-base\Kconfg-language.txt.svn-base'

 

On my computer a folder with some already downloaded files was created. What am I doing wrong and how to avoid it or override?

QuoteReplyEditDelete

 

 

2008-03-05 15:18:58     Re: Error while downloading svn

Mike Frysinger (UNITED STATES)

Message: 52130    what filesystem are downloading to ?  you cannot checkout on a case-insensitive filesystem

QuoteReplyEditDelete

 

 

2008-03-06 08:59:42     Re: Error while downloading svn

Ivan Koryakovskiy (RUSSIAN FEDERATION)

Message: 52156    Mike, you mean I have to use linux to checkout? currently I use windows as a primary OS and linux on a virtual Machine.

QuoteReplyEditDelete

 

 

2008-03-06 10:24:18     Re: Error while downloading svn

Mike Frysinger (UNITED STATES)

Message: 52161    you cannot checkout things in windows ... you have to use linux.  whether you use linux in a virtual machine or natively does not matter.  you have to check things out onto a native partition as well -- one that is case sensitive.

Attachments

    Outcomes