FAQ: EVAL-ADIS External Supply

Document created by NevadaMark Employee on Sep 16, 2013
Version 1Show Document
  • View in full screen mode

Q:

Can I connect my device-under-test (DUT) to an external power supply using the EVAL-ADIS?

A:

--------------------------------------------------------------------------------------------------------------------------------------

Yes, set JP1 to "EXT" and connect J3 to the external power supply, using the following figure as a guideline. Note that these inputs provide direct access to the DUT, which often do not have transient or reverse-insertion protection.  Device damage, due to over-stress, is not covered under warranty.

EVAL-ADIS-ExtVDD2.jpg

Attachments

    Outcomes