[#7330] l1 app test on uclinux-dist head fails

Document created by Aaronwu Employee on Sep 12, 2013
Version 1Show Document
  • View in full screen mode

[#7330] l1 app test on uclinux-dist head fails

Submitted By: Mingquan Pan

Open Date

2012-09-13 05:22:55     Close Date

2012-10-18 03:04:47

Priority:

Medium     Assignee:

Bob Liu

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Assigned (Not Start)

Uboot version or rev.:

    Toolchain version or rev.:

trunk head

App binary format:

N/A     

Summary: l1 app test on uclinux-dist head fails

Details:

 

l1 app test on uclinux-dist head fails.

 

## Booting kernel from Legacy Image at 02000000 ...

   Image Name:   bf537-0.2-3.5.0-ADI-2012R1-pre-0

   Created:      2012-09-12  15:08:04 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    4836069 Bytes = 4.6 MiB

   Load Address: 00001000

   Entry Point:  001cfd0c

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 001cfd0c

Linux version 3.5.0-ADI-2012R1-pre-00842-g0de3a1e (test@uclinux55-bf537-cf) (gcc version 4.3.5 (ADI-trunk/svn-5865) ) #34 Wed Sep 12 23:07:47 CST 2012

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Limiting kernel memory to 56MB due to anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0013a248

  rodata    = 0x0013a248-0x0019c8fc

  bss       = 0x0019d000-0x001ad5a0

  data      = 0x001ad5a0-0x001c8000

    stack   = 0x001c6000-0x001c8000

  init      = 0x001c8000-0x00900000

  available = 0x00900000-0x03800000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace active and enabled

Boot Mode: 0

Reset caused by Software reset

Blackfin support (C) 2004-2010 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 125 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14224

Kernel command line: root=/dev/mtdblock0 rw ip=10.100.4.50 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50:10.100.4.174:192.168.0.1:255.255.255.0:bf537-stamp:eth0:off

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 47520k/65536k RAM, (7392k init code, 1252k kernel code, 568k data, 1024k dma, 7780k reserved)

NR_IRQS:146

Configuring Blackfin Priority Driven Interrupts

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Calibrating delay loop... 995.32 BogoMIPS (lpj=1990656)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (34 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

bio: create slab <bio-0> at 0

bfin-spi bfin-spi.0: master is unqueued, this is deprecated

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs@ffc00500, dma channel@7

Switching to clocksource bfin_cs_cycles

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP: reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

debug-mmrs: setting up Blackfin MMR debugfs

msgmni has been set to 92

io scheduler noop registered (default)

bfin-uart: Blackfin serial driver

bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=bfin_mii_bus-0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)

bfin_mac bfin_mac.0: eth0: Blackfin on-chip Ethernet MAC driver, Version 1.1

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin_wdt: initialized: timeout=20 sec (nowayout=0)

TCP: cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-12-12 11:14:09 UTC (29848449)

IP-Config: Gateway not on directly connected network

dma_alloc_init: dma_page @ 0x027d3000 - 256 pages at 0x03f00000ýFreeing unused kernel memory: 7392k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.18.4 (2012-09-12 17:09:43 CST) hush - the humble shell

 

root:/> version

kernel:    Linux release 3.5.0-ADI-2012R1-pre-00842-g0de3a1e, build #34 Wed Sep 12 23:07:47 CST 2012

toolchain: bfin-uclinux-gcc release gcc version 4.3.5 (ADI-trunk/svn-5865)

user-dist: release svn-10799, build #382 Wed Sep 12 23:04:55 CST 2012

root:/> successful boot attempt

************** STEP 3: Start testing.

 

PHY: bfin_mii_bus-0:01 - Link is Up - 100/Full

ifconfig eth0 10.100.4.50 up

root:/>

PASS: Clean src directory

spawn make

bfin-linux-uclibc-gcc -shared -o libhelloworld.so helloworld.c -fno-jump-tables -mfdpic -Wl,--sep-code -Wl,--code-in-l1 -Wl,-z -Wl,now -Wl,--data-in-l1

bfin-linux-uclibc-gcc -pie -o test_helloworld test_helloworld.c -lhelloworld -L./ -fno-jump-tables -mfdpic

bfin-linux-uclibc-g++ -shared -o libhelloworldcpp.so helloworld.cpp -fno-jump-tables -mfdpic

/opt/uClinux.2012_Sep_11_18_12/bfin-linux-uclibc/bin/../lib/gcc/bfin-linux-uclibc/4.3.5/../../../../bfin-linux-uclibc/bin/ld: fde encoding in /tmp/ccyIP5iL.o(.eh_frame) prevents .eh_frame_hdr table being created.

bfin-linux-uclibc-g++ -o test_helloworldcpp test_helloworld.cpp -lhelloworldcpp -L./ -fno-jump-tables -mfdpic

 

PASS: Build test program

 

Case 2 ...PASS

 

Case 2 ...PASS

 

PASS: Copy libhelloworld.so to target board

 

PASS: Copy libhelloworldcpp.so to target board

 

PASS: Copy test_helloworld to target board

 

taskset 1 ./test_helloworld

root:/>

Last passed time: 2012_Sep_09_16_41.

Uclinux-dist version: 10797.

Kernel verion: , Git-id is not found!

 

 

Follow-ups

 

--- Mingquan Pan                                             2012-10-18 04:06:30

It passes after kernel source updated to trunk head. Close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes