[#7284] Can't detect ad1836 on bf537-stamp in latest trunk

Document created by Aaronwu Employee on Sep 12, 2013
Version 1Show Document
  • View in full screen mode

[#7284] Can't detect ad1836 on bf537-stamp in latest trunk

Submitted By: Vivi Li

Open Date

2012-08-24 03:35:48    

Priority:

Medium     Assignee:

Scott Jiang

Status:

Open     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3-2012_Aug_09

App binary format:

N/A     

Summary: Can't detect ad1836 on bf537-stamp in latest trunk

Details:

 

Can't detect ad1836 on bf537-stamp.

 

--

Linux version 3.5.0-ADI-2012R1-pre-00825-ga1810c5 (test@uclinux50-bf537-9960-1836) (gcc version 4.3.5 (ADI-2012R1-RC2) ) #685 Th2

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Limiting kernel memory to 56MB due to anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x00164c58

  rodata    = 0x00164c58-0x001d3b18

  bss       = 0x001d4000-0x001e4fe0

  data      = 0x001e4fe0-0x00200000

    stack   = 0x001fe000-0x00200000

  init      = 0x00200000-0x00923000

  available = 0x00923000-0x03800000

  DMA Zone  = 0x03e00000-0x04000000

Hardware Trace active and enabled

Boot Mode: 0

Reset caused by Software reset

Blackfin support (C) 2004-2010 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 125 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14224

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50f

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 47380k/65536k RAM, (7308k init code, 1423k kernel code, 621k data, 2048k dma, 6756k reserved)

NR_IRQS:146

Configuring Blackfin Priority Driven Interrupts

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Calibrating delay loop... 995.32 BogoMIPS (lpj=1990656)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (34 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

bio: create slab <bio-0> at 0

bfin-spi bfin-spi.0: master is unqueued, this is deprecated

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs@ffc00500, dma channel@7

Advanced Linux Sound Architecture Driver Version 1.0.25.

Switching to clocksource bfin_cs_cycles

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP: reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

debug-mmrs: setting up Blackfin MMR debugfs

msgmni has been set to 92

io scheduler noop registered (default)

bfin-uart: Blackfin serial driver

bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=bfin_mii_bus-0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125M)

bfin_mac bfin_mac.0: eth0: Blackfin on-chip Ethernet MAC driver, Version 1.1

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin_wdt: initialized: timeout=20 sec (nowayout=0)

bfin-tdm bfin-tdm.0: dma rx:3 tx:4, err irq:45, regs:ffc00800

TCP: cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-02-21 00:57:19 UTC (4409839)

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174

     host=bf537-stamp, domain=, nis-domain=(none)

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

ALSA device list:

  No soundcards found.

dma_alloc_init: dma_page @ 0x02964000 - 512 pages at 0x03e00000ýFreeing unused kernel memory: 7308k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.18.4 (2012-08-23 09:20:38 CST) hush - the humble shell

 

root:/> PHY: bfin_mii_bus-0:01 - Link is Up - 100/Full

 

root:/> version

kernel:    Linux release 3.5.0-ADI-2012R1-pre-00825-ga1810c5, build #685 Thu Aug 23 09:22:42 CST 2012

toolchain: bfin-linux-uclibc-gcc release gcc version 4.3.5 (ADI-2012R1-RC2)

user-dist: release svn-10780, build #9924 Thu Aug 23 09:22:06 CST 2012

root:/>

--

 

Follow-ups

 

--- Scott Jiang                                              2012-09-05 04:48:18

fixed.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.linux.audio_ad1836    application/octet-stream    40160    Vivi Li

Outcomes