[#7228] Fail to wake up when usb device is enabled on bf548/bf527

Document created by Aaronwu Employee on Sep 12, 2013
Version 1Show Document
  • View in full screen mode

[#7228] Fail to wake up when usb device is enabled on bf548/bf527

Submitted By: Vivi Li

Open Date

2012-08-06 05:50:44     Close Date

2012-08-24 02:44:47

Priority:

Medium     Assignee:

Bob Liu

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3-2012_Feb_15

App binary format:

N/A     

Summary: Fail to wake up when usb device is enabled on bf548/bf527

Details:

 

Fail to wake up when usb device is enabled on bf548/bf527.

 

Last passed time: 2012_Jun_18_03_21

--

kernel:    Linux release 3.3.0-ADI-2012R1-pre-00745-g458338c, build #144 Mon Jun 18 13:08:58 CST 2012

toolchain: bfin-uclinux-gcc release gcc version 4.3.5 (ADI-trunk/svn-5764)

user-dist: release svn-10716, build #143 Mon Jun 18 13:08:11 CST 2012

--

 

First failed time: 2012_Jun_19_03_5

--

kernel:    Linux release 3.3.0-ADI-2012R1-pre-00750-gd7def46, build #156 Tue Jun 19 13:31:30 CST 2012

toolchain: bfin-uclinux-gcc release gcc version 4.3.5 (ADI-trunk/svn-5764)

user-dist: release svn-10717, build #154 Tue Jun 19 13:30:44 CST 2012

--

 

Bellow is the error log:

--

Linux version 3.3.0-ADI-2012R1-pre-00750-gd7def46 (test@uclinux62-548-usbdev) (gcc version 4.3.5 (ADI-trunk/svn-5764) ) #156 Tue2

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart1] enabled

early printk enabled on early_BFuart1

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x001cd780

  rodata    = 0x001cd780-0x00269fb4

  bss       = 0x0026a000-0x0027c0e4

  data      = 0x0027c0e4-0x0029a000

    stack   = 0x00298000-0x0029a000

  init      = 0x0029a000-0x00a49000

  available = 0x00a49000-0x03e00000

  DMA Zone  = 0x03e00000-0x04000000

Hardware Trace active and enabled

Boot Mode: 1

Reset caused by Software reset

Blackfin support (C) 2004-2010 Analog Devices, Inc.

Compiled for ADSP-BF548 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 525 MHz core clock and 131 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

  L2 SRAM        : uncacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-through) in data cache

  L2 SRAM        : uncacheable in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 15748

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart1,57600 console=tty0 console=ttyBF1,57600 if

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 52348k/65536k RAM, (7868k init code, 1841k kernel code, 819k data, 2048k dma, 612k reserved)

NR_IRQS:295

Configuring Blackfin Priority Driven Interrupts

Šconsole [ttyBF1] enabled, bootconsole disabledrly

console [ttyBF1] enabled, bootconsole disabled

Calibrating delay loop... 1044.48 BogoMIPS (lpj=2088960)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (41 KB free)

Blackfin L2 SRAM: 128 KB (128 KB free)

NET: Registered protocol family 16

gpiochip_add: registered GPIOs 0 to 159 on device: BFIN-GPIO

Blackfin DMA Controller

ezkit_init(): registering device resources

bio: create slab <bio-0> at 0

SCSI subsystem initialized

spi spi0.2: Warning: SPI CPHA not set: Slave Select not under software control!

See Documentation/blackfin/bfin-spi-notes.txt

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs@ffc00500, dma channel@4

bfin-spi bfin-spi.1: Blackfin on-chip SPI Controller Driver, Version 1.0, regs@ffc02300, dma channel@5

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc00700

i2c-bfin-twi i2c-bfin-twi.1: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc02200

Advanced Linux Sound Architecture Driver Version 1.0.24.

musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)

musb-hdrc: kernel must blacklist external hubs

musb-hdrc musb-hdrc: USB OTG mode controller at ffc03c00 using DMA, IRQ 82

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

debug-mmrs: setting up Blackfin MMR debugfs

msgmni has been set to 102

io scheduler noop registered (default)

bf54x-lq043: FrameBuffer initializing...

dma_alloc_init: dma_page @ 0x02a4a000 - 512 pages at 0x03e00000

bfin-uart: Blackfin serial driver

bfin-uart.1: ttyBF1 at MMIO 0xffc02000 (irq = 48) is a BFIN-UART

bfin-otp: initialized

brd: module loaded

register bfin atapi driver

scsi0 : pata-bf54x

ata1: PATA max UDMA/66 irq 68

physmap platform flash device: 02000000 at 20000000

physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID 0x000089 Chip ID 0x00881e

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Using buffer write method

Using auto-unlock on power-up/resume

cfi_cmdset_0001: Erase suspend on write enabled

Creating 5 MTD partitions on "physmap-flash.0":

0x000000000000-0x000000080000 : "bootloader(nor)"

0x000000080000-0x000000480000 : "linux kernel(nor)"

0x000000480000-0x000000fe0000 : "file system(nor)"

0x000000fe0000-0x000000ff8000 : "config(nor)"

0x000000ff8000-0x000001000000 : "u-boot env(nor)"

m25p80 spi0.1: m25p16 (2048 Kbytes)

Creating 2 MTD partitions on "m25p80":

0x000000000000-0x000000080000 : "bootloader(spi)"

ata1.00: ATA-7: FUJITSU MHW2040AT, 0000000B, max UDMA/100

ata1.00: 78140160 sectors, multi 16: LBA

0x000000080000-0x000000200000 : "linux kernel(spi)"

BF5xx on-chip NAND FLash Controller Driver, Version 1.2 (c) 2007 Analog Devices, Inc.

bf5xx-nand bf5xx-nand.0: data_width=8, wr_dly=3, rd_dly=3

NAND device: Manufacturer ID: 0x20, Chip ID: 0xda (ST Micro NAND 256MiB 3,3V 8-bit)

ata1.00: configured for UDMA/66

scsi 0:0:0:0: Direct-Access     ATA      FUJITSU MHW2040A 0000 PQ: 0 ANSI: 5

sd 0:0:0:0: [sda] 78140160 512-byte logical blocks: (40.0 GB/37.2 GiB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA

Creating 3 MTD partitions on "NAND 256MiB 3,3V 8-bit":

0x000000000000-0x000000080000 : "bootloader(nand)"

0x000000080000-0x000000480000 : "linux kernel(nand)"

0x000000480000-0x000010000000 : "file system(nand)"

smsc911x: Driver version 2008-10-21

smsc911x-mdio: probed

smsc911x smsc911x.0: eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=smsc911x-0:01, irq=-1)

smsc911x smsc911x.0: eth0: MAC Address: 00:e0:22:fe:bd:09

input: bf54x-keys as /devices/platform/bf54x-keys/input/input0

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

i2c /dev entries driver

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

ALSA device list:

  No soundcards found.

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1987-09-23 08:52:50 UTC (559385570)

smsc911x smsc911x.0: eth0: SMSC911x/921x identified at 0x24000000, IRQ: 175

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf548-ezkit, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

mmc0: host does not support reading read-only switch. assuming write-enable.

mmc0: new SD card at address e624

sda: sda1

sd 0:0:0:0: [sda] Attached SCSI disk

Freeing unused kernel memory: 7868k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.18.4 (2012-06-19 04:05:17 CST) hush - the humble shell

 

root:/> dd if=/dev/zero of=fsg.block bs=1M count=16

16+0 records in

16+0 records out

root:/> modprobe g_file_storage file=/fsg.block stall=0

gadget: No serial-number string provided!

gadget: File-backed Storage Gadget, version: 1 September 2010

gadget: NOTE: This driver is deprecated.  Consider using g_mass_storage instead.

gadget: Number of LUNs=1

g_file_storage gadget-lun0: ro=0, nofua=0, file: /fsg.block

musb-hdrc musb-hdrc: MUSB HDRC host driver

musb-hdrc musb-hdrc: new USB bus registered, assigned bus number 1

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

root:/>  gadget: high-speed config #1

 

root:/>

root:/> rtcwake -s 10 -m standby

wakeup from "standby" at Wed Sep 23 09:03:53 1987

PM: Syncing filesystems ... done.

mmc0: card e624 removed

Freezing user space processes ... (elapsed 0.01 seconds) done.

Freezing remaining freezable tasks ... (elapsed 0.01 seconds) done.

Suspending console(s) (use no_console_suspend to debug)

--

 

Follow-ups

 

--- Bob Liu                                                  2012-08-22 06:19:09

fixed, Shouldn't poll for MUSB_DEVCTL when peripheral mode is enabled.

 

--- Vivi Li                                                  2012-08-24 03:43:11

OK, close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.config.power_usbdev.dma    application/octet-stream    51993    Vivi Li

config.linux.power_usbdev.dma    application/octet-stream    53801    Vivi Li

Outcomes