[#7220] bonnie++ test on bf548 ezkit sdiommc fails with kernel panic

Document created by Aaronwu Employee on Sep 12, 2013
Version 1Show Document
  • View in full screen mode

[#7220] bonnie++ test on bf548 ezkit sdiommc fails with kernel panic

Submitted By: Mingquan Pan

Open Date

2012-07-31 05:04:34     Close Date

2012-08-15 23:05:07

Priority:

Medium     Assignee:

Sonic Zhang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

BF548     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Assigned (Not Start)

Uboot version or rev.:

    Toolchain version or rev.:

ADI-trunk/svn-5764

App binary format:

N/A     

Summary: bonnie++ test on bf548 ezkit sdiommc fails with kernel panic

Details:

 

bonnie++ test on bf548 ezkit sdiommc fails with kernel panic now.

 

time bonnie++ -u root -d /mnt -s 200M^M

Using uid:0, gid:0.^M

Writing a byte at a time...done^M

Writing intelligently...INFO: task kworker/u:2:202 blocked for more than 120 seconds.^M

"echo 0 > /proc/sys/kernel/hung_task_timeout_secs" disables this message.^M

kworker/u:2     D ffa009d8     0   202      2 0x00000000^M

Stack info:^M

SP: [0x02a6be70] <0x02a6be70> /* kernel dynamic memory */^M

FP: (0x02a6bfa0)^M

Memory from 0x02a6be70 to 02a6c000^M

02a6be70:[00000000] 02058190  00000000  02058040  02a93820  02a5b360  00000002  02a6beac ^M

02a6be90: 001cd17c  00000000  00000008  00000000  02a6a008  02a6a000  02a6a000  0000003f ^M

02a6beb0: 0014267c  02a6a000  02a92200  02a6a000  02071405  0000ffff  00000001  00000002 ^M

02a6bed0: 0025ace0  0000ffff  00143538  02071400  02a92344  00000000  02058040  00028500 ^M

02a6bef0: 02a92344  02a92344  0024cba8  00146608  02a92200  02a5eb60  0025ace0  02071405 ^M

02a6bf10: 00143538  02071400  00000000  000292a2  00000000  02058190 <00143708> 02a92200 ^M

02a6bf30: 02071405  02058040  02a6bf64  001cd18a <0001c7b8> 02a92354  02a5eb60  0025ace0 ^M

02a6bf50: 02071405  00000000  02a6a008  02a6a000  02a6a000  0025ace0  0001d1a8  02a5eb60 ^M

02a6bf70: 0024cba8  00000000  02a5eb70  02a5eb70  0025d754  0024cba0  02045f00  0001d080 ^M

02a6bf90: 00000000  02a6a000  02a6a000  02a6a000 (00000000)<00021004> 02045f00  0001d080 ^M

02a6bfb0: 00000000  02a5eb60  00000000  00000000  00000000  00000000  00000000  00020fa0 ^M

02a6bfd0: 00000000  02a5eb60  00000000  02a6bfdc  02a6bfdc <0000161e> 00000000  00000000 ^M

02a6bff0: 00000000  00000000  ffffffff  00000006 ^M

Return addresses in stack:^M

------------[ cut here ]------------^M

kernel BUG at kernel/kallsyms.c:215!^M

Kernel panic - not syncing: BUG()^M

Hardware Trace:^M

Double Fbonnie++ failed

 

Last passed time: 2012_Jul_23_01_49.

Uclinux-dist version: 10741.

Kernel verion: , Git-id is not found!

 

Case 33 ...FAIL

 

 

Follow-ups

 

--- Mingquan Pan                                             2012-08-16 00:03:46

It passes now. Close.

 

root:/> ^[[6nversion^M

kernel:    Linux release 3.5.0-ADI-2012R1-pre-00813-g6696c85, build #18 Sat Aug

11 05:36:18 CST 2012^M

toolchain: bfin-uclinux-gcc release gcc version 4.3.5 (ADI-2012R1-RC2) ^M

user-dist: release svn-10769, build #242 Sat Aug 11 05:35:18 CST 2012^M

root:/> ^[[6nsuccessful boot attemptfdisk /dev/mmcblk0^M

 

Case 32 ...PASS

 

Case 32 ...PASS

^[[6necho 0 > /proc/sys/kernel/hung_task_timeout_secs^M

root:/> ^[[6ntime bonnie++ -u root -d /mnt -s 200M^M

Using uid:0, gid:0.^M

Writing a byte at a time...done^M

Writing intelligently...done^M

Rewriting...done^M

Reading a byte at a time...done^M

Reading intelligently...done^M

start 'em...done...done...done...done...done...^M

Create files in sequential order...done.^M

Stat files in sequential order...done.^M

Delete files in sequential order...done.^M

Create files in random order...done.^M

Stat files in random order...done.^M

Delete files in random order...done.^M

Version  1.94       ------Sequential Output------ --Sequential Input-

--Random-^M

Concurrency   1     -Per Chr- --Block-- -Rewrite- -Per Chr- --Block--

--Seeks--^M

Machine        Size K/sec %CP K/sec %CP K/sec %CP K/sec %CP K/sec %CP  /sec

%CP^M

blackfin       200M    70  95   996   3   861   3   171  99  5027  13  91.5 

3^M

Latency               767ms     600ms     792ms   52000us   44000us  

6895ms^M

Version  1.94       ------Sequential Create------ --------Random

Create--------^M

blackfin            -Create-- --Read--- -Delete-- -Create-- --Read---

-Delete--^M

              files  /sec %CP  /sec %CP  /sec %CP  /sec %CP  /sec %CP  /sec

%CP^M

                 16   335  88 19598 100  2533  30   339  89 27675  99   822

63^M

Latency             15999us    4000us    4000us   19999us    4000us  

8000us^M

1.93c,1.94,blackfin,1,1086004771,200M,,70,95,996,3,861,3,171,99,5027,13,91.5,3,16,,,,,335,88,19598,100,2533,30,339,89,27675,99,822,63,767ms,600ms,792ms,52000us,44000us,6895ms,15999us,4000us,4000us,19999us,4000us,8000us^M

real    12m 43.92s^M

user    0m 13.90s^M

sys     2m 54.05s^M

root:/> ^[[6n

Case 33 ...PASS

 

Case 33 ...PASS

 

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes