FAQ: [#7210] ad73311 build fail after update kernel to 3.5(2012)

Document created by Aaronwu Employee on Sep 12, 2013
Version 1Show Document
  • View in full screen mode

[#7210] ad73311 build fail after update kernel to 3.5

Submitted By: Bob Liu

Open Date

2012-07-26 03:51:24     Close Date

2012-09-07 03:46:51

Priority:

Medium     Assignee:

Scott Jiang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

snaps     Release:

trunk

Category:

N/A     Board:

STAMP

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc version 4.3.5 (ADI-2012R1-

App binary format:

N/A     

Summary: ad73311 build fail after update kernel to 3.5

Details:

 

  LD      sound/soc/codecs/built-in.o

  CC [M]  sound/soc/codecs/ad73311.o

sound/soc/codecs/ad73311.c: In function ‘ad73311_soc_probe’:

sound/soc/codecs/ad73311.c:157: error: implicit declaration of function ‘snd_soc_add_controls’

make[3]: *** [sound/soc/codecs/ad73311.o] Error 1

make[2]: *** [sound/soc/codecs] Error 2

make[1]: *** [sound/soc] Error 2

make: *** [sound] Error 2

root@bob-OptiPlex-760:/old/home/bob/linux-kernel-git/linux-kernel#

 

snd_soc_add_controls has been removed(renamed?) in framework.

 

Follow-ups

 

--- James Kosin                                              2012-08-07 12:32:24

I'm getting the same from trunk.

 

It looks like we need to change to use the appropriate new functions to perform

the tasks:

snd_soc_add_codec_controls()

snd_soc_add_platform_controls()

snd_soc_add_card_controls()

snd_soc_add_dai_controls()

 

--- James Kosin                                              2012-08-07 14:25:06

This problem affects the following drivers:

sound/soc/codec/adau17x1.c

sound/soc/codec/adau1761.c

sound/soc/codec/ad73311.c

 

 

--- James Kosin                                              2012-08-07 14:25:17

This problem affects the following drivers:

sound/soc/codec/adau17x1.c

sound/soc/codec/adau1761.c

sound/soc/codec/ad73311.c

 

 

--- Scott Jiang                                              2012-08-10 02:31:19

fixed.

 

--- Vivi Li                                                  2012-09-07 04:46:59

OK in trunk. Close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes