FAQ:[#7157] Fail to compile enc28j60 for spi net test in trunk(2012)

Document created by Aaronwu Employee on Sep 12, 2013
Version 1Show Document
  • View in full screen mode

[#7157] Fail to compile enc28j60 for spi net test in trunk

Submitted By: Vivi Li

Open Date

2012-06-13 05:39:44     Close Date

2012-06-19 05:28:18

Priority:

Medium     Assignee:

Bob Liu

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

Make Errors     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3-2012_Feb_15

App binary format:

N/A     

Summary: Fail to compile enc28j60 for spi net test in trunk

Details:

 

Fail to compile enc28j60 for spi net test in trunk.

 

I can find both drivers/net/ethernet/microchip/enc28j60.c and drivers/net/enc28j60.c use enc28j60_hw.h. These two C files are very similar. Are they duplicated?

--

test@uclinux50:linux-2.6.x> grep -nr "enc28j60_hw.h" .

./drivers/net/ethernet/microchip/enc28j60_hw.h:2: * enc28j60_hw.h: EDTP FrameThrower style enc28j60 registers

./drivers/net/ethernet/microchip/enc28j60_hw.h:4: * $Id: enc28j60_hw.h,v 1.9 2007/12/14 11:59:16 claudio Exp $

./drivers/net/ethernet/microchip/enc28j60.c:32:#include "enc28j60_hw.h"

./drivers/net/enc28j60.c:32:#include "enc28j60_hw.h"

test@uclinux50:linux-2.6.x>

--

 

Bellow is the error log:

--

  CC      drivers/net/ethernet/microchip/enc28j60.o

  CC      drivers/net/enc28j60.o

drivers/net/enc28j60.c:32:25: error: enc28j60_hw.h: No such file or directory

drivers/net/enc28j60.c:75: error: ‘MAX_FRAMELEN’ undeclared here (not in a function)

drivers/net/enc28j60.c: In function ‘spi_read_buf’:

drivers/net/enc28j60.c:100: error: ‘ENC28J60_READ_BUF_MEM’ undeclared (first use in this function)

drivers/net/enc28j60.c:100: error: (Each undeclared identifier is reported only once

drivers/net/enc28j60.c:100: error: for each function it appears in.)

drivers/net/enc28j60.c: In function ‘spi_write_buf’:

drivers/net/enc28j60.c:128: error: ‘ENC28J60_WRITE_BUF_MEM’ undeclared (first use in this function)

drivers/net/enc28j60.c: In function ‘spi_read_op’:

drivers/net/enc28j60.c:151: error: ‘SPRD_MASK’ undeclared (first use in this function)

drivers/net/enc28j60.c:154: error: ‘ADDR_MASK’ undeclared (first use in this function)

drivers/net/enc28j60.c: In function ‘spi_write_op’:

drivers/net/enc28j60.c:173: error: ‘ADDR_MASK’ undeclared (first use in this function)

drivers/net/enc28j60.c: In function ‘enc28j60_soft_reset’:

drivers/net/enc28j60.c:187: error: ‘ENC28J60_SOFT_RESET’ undeclared (first use in this function)

drivers/net/enc28j60.c: In function ‘enc28j60_set_bank’:

drivers/net/enc28j60.c:198: error: ‘BANK_MASK’ undeclared (first use in this function)

...

--

 

Follow-ups

 

--- Bob Liu                                                  2012-06-18 05:03:43

fixed,

 

--- Vivi Li                                                  2012-06-19 06:29:27

OK now. Close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.linux.spi_net    application/octet-stream    37903    Vivi Li

Attachments

Outcomes