FAQ: [#7091] bf548-ezkit kernel fail to boot in latest trunk(2012)

Document created by Aaronwu Employee on Sep 12, 2013
Version 1Show Document
  • View in full screen mode

[#7091] bf548-ezkit kernel fail to boot in latest trunk

Submitted By: Vivi Li

Open Date

2012-04-28 05:44:13     Close Date

2012-05-09 22:39:41

Priority:

Medium High     Assignee:

steven miao

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

EZKIT Lite

Processor:

BF548     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3-2012_Feb_15_10_55

App binary format:

N/A     

Summary: bf548-ezkit kernel fail to boot in latest trunk

Details:

 

bf548-ezkit kernel fail to boot in latest trunk.

 

Last passed time: 2012_Apr_19_07_11

--

kernel:    Linux release 3.3.0-ADI-2012R1-pre-00364-g31a7cfc, build #186 Thu Apr 19 15:52:34 CST 2012

toolchain: bfin-uclinux-gcc release gcc version 4.3.5 (ADI-trunk/svn-5764)

user-dist: release svn-10654, build #2991 Thu Apr 19 15:51:44 CST 2012

--

 

Bellow is the error log:

--

U-Boot 2011.09-dirty (ADI-2011R1) (Nov 10 2011 - 17:53:02)

 

CPU:   ADSP bf548-0.0 (Detected Rev: 0.2) (parallel flash boot)

Board: ADI BF548 EZ-Kit board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 525 MHz, Core: 525 MHz, System: 131.250 MHz

RAM:   64 MiB

 

RAM size is 64 MB.

Flash: 16 MiB

NAND:  256 MiB

MMC:   Blackfin SDH: 0

In:    serial

Out:   serial

Err:   serial

KGDB:  [on serial] ready

Net:   smc911x-0

Hit any key to stop autoboot:  5 ^H^H^H 0

bfin> set bootargs root=/dev/mtdblock0 rw ip=10.100.4.50 earlyprintk=serial,uart1,57600 console=ttyBF1,57600

bfin> set serverip 10.100.4.174

bfin> set ipaddr 10.100.4.50

bfin> save

Saving Environment to Flash...

. done

Un-Protected 1 sectors

Erasing Flash...

. done

Erased 1 sectors

Writing to Flash... 9....8....7....6....5....4....3....2....1....done

. done

Protected 1 sectors

bfin> printenv ethaddr

ethaddr=00:E0:22:FE:BF:4E

bfin> mac address=00:E0:22:FE:BF:4E

tftpboot 0x2000000 uImage

smc911x: detected LAN9218 controller

smc911x: phy initialized

smc911x: MAC 00:e0:22:fe:bf:4e

Using smc911x-0 device

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'uImage'.

Load address: 0x2000000

Loading: *^H#################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         ##########################################

done

Bytes transferred = 5387459 (5234c3 hex)Image size is 5234c3

 

bfin> run addip

bfin> bootm

## Booting kernel from Legacy Image at 02000000 ...

   Image Name:   bf548-0.2-3.3.0-ADI-2012R1-pre-0

   Created:      2012-04-27  22:25:09 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    5387395 Bytes = 5.1 MiB

   Load Address: 00001000

   Entry Point:  00283e90

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 00283e90

--

 

Follow-ups

 

--- steven miao                                              2012-05-08 02:40:41

fix peripheral pin request hang on bf548

 

--- Vivi Li                                                  2012-05-09 23:38:24

OK now.

Close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.policy    application/octet-stream    45888    Vivi Li

Attachments

Outcomes