FAQ: [#7077] ide harddisk test now fails at bonnie ++ for can't read data(2012)

Document created by Aaronwu Employee on Sep 12, 2013
Version 1Show Document
  • View in full screen mode

[#7077] ide harddisk test now fails at bonnie ++ for can't read data

Submitted By: Mingquan Pan

Open Date

2012-04-26 23:02:05    

Priority:

Low     Assignee:

Bob Liu

Status:

Open     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Assigned (Not Start)

Uboot version or rev.:

    Toolchain version or rev.:

ADI-trunk/svn-5764

App binary format:

N/A     

Summary: ide harddisk test now fails at bonnie ++ for can't read data

Details:

 

ide cdrom fails to be recognized on trunk head now.

 

scsi0 : pata_platform^M

ata1: PATA max PIO0 mmio cmd 0x20314020 ctl 0x2031401c irq 55^M

bfin_mii_bus: probed^M

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=bfin_mii_bus-0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)^M

bfin_mac bfin_mac.0: eth0: Blackfin on-chip Ethernet MAC driver, Version 1.1^M

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0^M

bfin-wdt: initialized: timeout=20 sec (nowayout=0)^M

TCP cubic registered^M

NET: Registered protocol family 17^M

rtc-bfin rtc-bfin: setting system clock to 1970-11-03 03:16:53 UTC (26450213)^M

IP-Config: Gateway not on directly connected network.^M

dma_alloc_init: dma_page @ 0x027f1000 - 256 pages at 0x03f00000^M

ata1.00: ATA-6: WDC WD800BB-00JHC0, 05.01C05, max UDMA/100^M

ata1.00: 156301488 sectors, multi 0: LBA ^M

ata1.01: ATAPI: TSSTcorpDVD-ROM TS-H352C, CH01, max UDMA/33^M

ata1.00: configured for PIO^M

ata1.01: configured for PIO^M

scsi 0:0:0:0: Direct-Access     ATA      WDC WD800BB-00JH 05.0 PQ: 0 ANSI: 5^M

ata1: WARNING: synchronous SCSI scan failed without making any progress, switching to async^M

Freeing unused kernel memory: 7404k freed^M

PHY: bfin_mii_bus-0:01 - Link is Up - 100/Full^M

scsi scan: INQUIRY result too short (5), using 36^M

root:/> ^[[6n

Case 1 ...PASS

 

Case 1 ...PASS

mount -t iso9660 /dev/sr0 /mnt^M

mount: mounting /dev/sr0 on /mnt failed: No such

Last passed time: 2012_Apr_19_10_15.

Uclinux-dist version: 10654.

Kernel verion: , Git-id is not found!

 

 

Follow-ups

 

--- Mingquan Pan                                             2012-06-05 06:41:23

This issue looks gone now and ide cdrom case is passed.

 

But instead ide harddisk fails for no device found frequently.

 

## Booting kernel from Legacy Image at 02000000 ...

   Image Name:   bf537-0.2-3.3.0-ADI-2012R1-pre-0

   Created:      2012-06-03  21:21:02 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    5100756 Bytes = 4.9 MiB

   Load Address: 00001000

   Entry Point:  00209c70

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 00209c70

Linux version 3.3.0-ADI-2012R1-pre-00705-g385282d (test@uclinux55-bf537-cf)

(gcc version 4.3.5 (ADI-trunk/svn-5764) ) #444 Mon Jun 4 05:20:41 CST 2012

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Limiting kernel memory to 56MB due to anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x001648e8

  rodata    = 0x001648e8-0x001dc150

  bss       = 0x001dd000-0x001edf4c

  data      = 0x001edf4c-0x00202000

    stack   = 0x00200000-0x00202000

  init      = 0x00202000-0x0096b000

  available = 0x0096b000-0x03800000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace active and enabled

Boot Mode: 0

Reset caused by Software reset

Blackfin support (C) 2004-2010 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 350 MHz core clock and 70 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14224

Kernel command line: root=/dev/mtdblock0 rw ip=10.100.4.50

earlyprintk=serial,uart0,57600 console=ttyBF0,57600

ip=10.100.4.50:10.100.4.174:192.168.0.1:255.255.255.0:bf537-stamp:eth0:off

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 47092k/65536k RAM, (7588k init code, 1422k kernel code, 630k

data, 1024k dma, 7780k reserved)

NR_IRQS:146

Configuring Blackfin Priority Driven Interrupts

start_kernel(): bug: interrupts were enabled early

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Calibrating delay loop... 697.34 BogoMIPS (lpj=1394688)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (34 KB free)

NET: Registered protocol family 16

gpiochip_add: registered GPIOs 0 to 47 on device: BFIN-GPIO

Blackfin DMA Controller

stamp_init(): registering device resources

bio: create slab <bio-0> at 0

SCSI subsystem initialized

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0,

regs@ffc00500, dma channel@7

Switching to clocksource bfin_cs_cycles

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

debug-mmrs: setting up Blackfin MMR debugfs

msgmni has been set to 91

io scheduler noop registered (default)

bfin-uart: Blackfin serial driver

bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

scsi0 : pata_platform

ata1: PATA max PIO0 mmio cmd 0x20314020 ctl 0x2031401c irq 55

bfin_mii_bus: probed

bfin_mac: attached PHY driver [Generic PHY]

(mii_bus:phy_addr=bfin_mii_bus-0:01, irq=-1,

mdc_clk=2500000Hz(mdc_div=13)@sclk=70MHz)

bfin_mac bfin_mac.0: eth0: Blackfin on-chip Ethernet MAC driver, Version 1.1

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-10-13 04:52:05 UTC (24641525)

IP-Config: Gateway not on directly connected network.

dma_alloc_init: dma_page @ 0x028a3000 - 256 pages at 0x03f00000ata1.00:

ATA-6: WDC WD800BB-00JHC0, 05.01C05, max UDMA/100

ata1.00: 156301488 sectors, multi 0: LBA

ata1.01: ATAPI: TSSTcorpDVD-ROM TS-H352C, CH01, max UDMA/33

ata1.00: configured for PIO

ata1.01: configured for PIO

scsi 0:0:0:0: Direct-Access     ATA      WDC WD800BB-00JH 05.0 PQ: 0 ANSI: 5

sd 0:0:0:0: [sda] 156301488 512-byte logical blocks: (80.0 GB/74.5 GiB)

scsi 0:0:1:0: CD-ROM            TSSTcorp DVD-ROM TS-H352C CH01 PQ: 0 ANSI: 5

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support

DPO or FUA

sda: sda1 sda2

sd 0:0:0:0: [sda] Attached SCSI disk

Freeing unused kernel memory: 7588k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.18.4 (2012-06-03 12:13:20 CST) hush - the humble shell

 

root:/> verPHY: bfin_mii_bus-0:01 - Link is Up - 100/Full

sion

kernel:    Linux release 3.3.0-ADI-2012R1-pre-00705-g385282d, build #444 Mon

Jun 4 05:20:41 CST 2012

toolchain: bfin-uclinux-gcc release gcc version 4.3.5 (ADI-trunk/svn-5764)

user-dist: release svn-10692, build #5932 Mon Jun 4 05:18:46 CST 2012

root:/> successful boot attempt

************** STEP 3: Start testing

 

dmesg|grep sd

sd 0:0:0:0: [sda] 156301488 512-byte logical blocks: (80.0 GB/74.5 GiB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Mode Sense: 00 3a 00 00

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support

DPO or FUA

sda: sda1 sda2

sd 0:0:0:0: [sda] Attached SCSI disk

root:/>

Case 1 ...PASS

 

Case 1 ...PASS

fdisk /dev/sda

 

The number of cylinders for this disk is set to 9729.

There is nothing wrong with that, but this is larger than 1024,

and could in certain setups cause problems with:

1) software that runs at boot time (e.g., old versions of LILO)

2) booting and partitioning software from other OSs

   (e.g., DOS FDISK, OS/2 FDISK)

 

Command (m for help): p

 

Disk /dev/sda: 255 heads, 63 sectors, 9729 cylinders

Units = cylinders of 16065 * 512 bytes

 

   Device Boot    Start       End    Blocks   Id  System

/dev/sda1             1        64    514048+  83  Linux

/dev/sda2            91       120    240975   83  Linux

 

Command (m for help): d

Partition number (1-4): 1

 

Command (m for help): n

Command action

   e   extended

   p   primary partition (1-4)

p

Partition number (1-4): 1

First cylinder (1-9729, default 1):

Using default value 1

Last cylinder or +size or +sizeM or +sizeK (1-90, default 90): +500M

 

Command (m for help): w

The partition table has been altered!

 

Calling ioctl() to re-read partition table.

sda: sda1 sda2

sda: sda1 sda2

 

WARNING: If you have created or modified any DOS 6.x

partitions, please see the fdisk manual page for additional

information.

Syncing disks.

 

Case 2 ...PASS

 

Case 2 ...PASS

root:/> mke2fs /dev/sda1

mke2fs 1.41.12 (17-May-2010)

Could not stat /dev/sda1 --- No such file or directory

 

The device apparently does not exist; did you specify it correctly?

root:/>

Last passed time: 2012_May_31_13_28.

Uclinux-dist version: 10688.

Kernel verion: , Git-id is not found!

 

Case 3 ...FAIL

 

 

And cf card is not found also:

bfin_cf_pcmcia bfin_cf_pcmcia: Blackfin CompactFlash/PCMCIA Socket Driver

bfin_cf_pcmcia bfin_cf_pcmcia: : on irq 54

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1971-01-12 07:47:33 UTC (32514453)

IP-Config: Gateway not on directly connected network.

dma_alloc_init: dma_page @ 0x028d8000 - 256 pages at 0x03f00000Freeing unused

kernel memory: 8324k freed

pcmcia_socket pcmcia_socket0: pccard: PCMCIA card inserted into slot 0

pcmcia 0.0: pcmcia: registering new device pcmcia0.0 (IRQ: 54)

scsi0 : pata_pcmcia

ata1: PATA max PIO0 cmd 0x20310000 ctl 0x2031000e irq 54

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...PHY: bfin_mii_bus-0:01 - Link is Up - 100/Full

 

 

BusyBox v1.18.4 (2012-06-03 12:13:20 CST) hush - the humble shell

 

root:/> version

kernel:    Linux release 3.3.0-ADI-2012R1-pre-00705-g385282d, build #447 Sun

Jun 3 20:25:10 CST 2012

toolchain: bfin-uclinux-gcc release gcc version 4.3.5 (ADI-trunk/svn-5764)

user-dist: release svn-10692, build #5905 Sun Jun 3 20:22:28 CST 2012

root:/> successful boot attempt

************** STEP 3: Start testing

 

dmesg|grep pcmcia

bfin_cf_pcmcia bfin_cf_pcmcia: Blackfin CompactFlash/PCMCIA Socket Driver

bfin_cf_pcmcia bfin_cf_pcmcia: : on irq 54

pcmcia_socket pcmcia_socket0: pccard: PCMCIA card inserted into slot 0

pcmcia 0.0: pcmcia: registering new device pcmcia0.0 (IRQ: 54)

scsi0 : pata_pcmcia

root:/>

Case 1 ...PASS

 

Case 1 ...PASS

pccardctl ident

Socket 0:

  product info: "SanDisk", "SDP", "5/3 0.6",

""

  manfid: 0x0045, 0x0401

  function: 4 (fixed disk)

root:/>

Case 2 ...PASS

 

Case 2 ...PASS

pccardctl status

Socket 0:

  3.3V 16-bit PC Card

  Subdevice 0 (function 0) bound to driver "pata_pcmcia"

root:/>

Case 3 ...PASS

 

Case 3 ...PASS

fdisk /dev/sda

 

Unable to open /dev/sda

root:/>

Last passed time: 2012_May_25_15_47.

Uclinux-dist version: 10685.

Kernel verion: , Git-id is not found!

 

Case 4 ...FAIL

 

 

--- Mingquan Pan                                             2012-10-18 06:06:27

ide harddisk test now fails at bonnie ++ timeout.

 

root:/> time bonnie++ -u root -d /mnt -s 200M^M

Using uid:0, gid:0.^M

Writing a byte at a time...done^M

Writing intelligently...done^M

Rewriting...done^M

Reading a byte at a time...done^M

Reading intelligently...done^M

start 'em...done...done...done...done...done...^M

Create files in sequential order...done.^M

Stat files in sequential order...Can't read data.^M

Cleaning up test directory after error.^M

Command exited with non-zero status 1^M

real    7m 20.91s^M

user    0m 17.44s^M

sys     5m 14.04s^M

root:/> ^[[6nbonnie++ timeout

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes