FAQ: [#6963] build usbotg fails at usb/musb/musb_core.c(2012)

Document created by Aaronwu Employee on Sep 12, 2013
Version 1Show Document
  • View in full screen mode

[#6963] build usbotg fails at usb/musb/musb_core.c

Submitted By: Mingquan Pan

Open Date

2012-02-02 02:57:20     Close Date

2012-05-14 05:28:03

Priority:

Medium     Assignee:

Bob Liu

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

BF527     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

2011r1-rc4

App binary format:

N/A     

Summary: build usbotg fails at usb/musb/musb_core.c

Details:

 

build usbotg fails at usb/musb/musb_core.c on bf527 ezkit.

 

  CC [M]  net/sunrpc/timer.o^M

  CC [M]  net/sunrpc/sunrpc_syms.o^M

  CC [M]  net/sunrpc/cache.o^M

  CC [M]  net/sunrpc/rpc_pipe.o^M

  CC [M]  net/sunrpc/svc_xprt.o^M

  CC [M]  net/sunrpc/stats.o^M

  LD [M]  net/sunrpc/sunrpc.o^M

  LD      net/built-in.o^M

  LD      vmlinux.o^M

  MODPOST vmlinux.o^M

  GEN     .version^M

  CHK     include/generated/compile.h^M

  UPD     include/generated/compile.h^M

  CC      init/version.o^M

  LD      init/built-in.o^M

  LD      .tmp_vmlinux1^M

drivers/built-in.o: In function `musb_free':^M

/home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x/drivers/usb/musb/musb_core.c:1841: undefined reference to `dma_controller_destroy'^M

drivers/built-in.o: In function `musb_init_controller':^M

/home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x/drivers/usb/musb/musb_core.c:1918: undefined reference to `dma_controller_create'^M

make[1]: *** [.tmp_vmlinux1] Error 1^M

make[1]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x'^M

make: *** [linux] Error 1^M

 

last known good version:

 

root:/> ^[[6nversion^M

kernel:    Linux release 3.2.0-ADI-2012R1-pre-svn10315, build #69 Wed Jan 18 16:36:28 CST 2012^M

toolchain: bfin-uclinux-gcc release gcc version 4.3.5 (ADI-2011R1-RC4) ^M

user-dist: release svn-10626, build #895 Wed Jan 18 16:35:09 CST 2012^M

 

Follow-ups

 

--- Bob Liu                                                  2012-02-06 04:09:00

fixed. updated default config

 

--- Mingquan Pan                                             2012-05-14 06:27:54

build usbotg ok now. Close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.linux.usbotg

Attachments

Outcomes