FAQ: [#6875] Netaudio fails to mount samba server in 2010r1 branch.(2011)

Document created by Aaronwu Employee on Sep 12, 2013
Version 1Show Document
  • View in full screen mode

[#6875] Netaudio fails to mount samba server in 2010r1 branch.

Submitted By: Vivi Li

Open Date

2011-11-10 05:13:15    

Priority:

Medium     Assignee:

Vivi Li

Aaron Wu

Status:

Open     Fixed In Release:

N/A

Found In Release:

2011R1     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Assigned (Not Start)

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3-2011R1-RC2

App binary format:

N/A     

Summary: Netaudio fails to mount samba server in 2010r1 branch.

Details:

 

Netaudio fails to mount samba server in 2010r1 branch.

I think we need to use cifs mount instead of smbmount.

Build script also needs upgrade.

 

--

U-Boot 2010.06-svn2487 (ADI-2010R1) (Oct 27 2010 - 04:28:50)

 

CPU:   ADSP bf537-0.2 (Detected Rev: 0.2) (bypass boot)

Board: ADI BF537 stamp board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 500 MHz, Core: 500 MHz, System: 125 MHz

RAM:   64 MiB

Flash: 4 MiB

In:    serial

Out:   serial

Err:   serial

KGDB:  [on serial] ready

Net:   bfin_mac

Hit any key to stop autoboot:  0

Using bfin_mac device

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'uImage'.

Load address: 0x1000000

Loading: #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #############################

done

Bytes transferred = 5192383 (4f3abf hex)

## Booting kernel from Legacy Image at 01000000 ...

   Image Name:   bf537-0.2-3.0.8-ADI-2011R1-svn10

   Created:      2011-11-10   3:15:03 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    5192319 Bytes = 5 MiB

   Load Address: 00001000

   Entry Point:  001dfc48

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 001dfc48

Linux version 3.0.8-ADI-2011R1-svn10145 (test@uclinux50-bf537-9960-1836) (gcc version 4.3.5 (ADI-2011R1-RC2) ) #66 Thu Nov 10 111

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Limiting kernel memory to 56MB due to anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x00149d78

  rodata    = 0x00149d78-0x001b3db4

  bss       = 0x001b4000-0x001c432c

  data      = 0x001c432c-0x001d8000

    stack   = 0x001d6000-0x001d8000

  init      = 0x001d8000-0x0096f000

  available = 0x0096f000-0x03800000

  DMA Zone  = 0x03e00000-0x04000000

Hardware Trace active and enabled

Boot Mode: 0

Blackfin support (C) 2004-2010 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 125 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14224

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50f

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 47076k/65536k RAM, (7772k init code, 1315k kernel code, 569k data, 2048k dma, 6756k reserved)

NR_IRQS:146

Configuring Blackfin Priority Driven Interrupts

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Calibrating delay loop... 995.32 BogoMIPS (lpj=1990656)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (35 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

bio: create slab <bio-0> at 0

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs@ffc00500, dma channel@7

Advanced Linux Sound Architecture Driver Version 1.0.24.

Switching to clocksource bfin_cs_cycles

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

debug-mmrs: setting up Blackfin MMR debugfs

msgmni has been set to 91

io scheduler noop registered (default)

bfin-uart: Blackfin serial driver

bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)

bfin_mac bfin_mac.0: eth0: Blackfin on-chip Ethernet MAC driver, Version 1.1

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

bfin-tdm bfin-tdm.0: dma rx:3 tx:4, err irq:45, regs:ffc00800

dma_alloc_init: dma_page @ 0x029d3000 - 512 pages at 0x03e00000

asoc: ad1836-hifi <-> bfin-tdm.0 mapping ok

ALSA device list:

  #0: bfin-ad1836

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-03 01:27:46 UTC (178066)

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf537-stamp, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 7772k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.18.4 (2011-11-10 11:11:01 CST) hush - the humble shell

 

root:/> PHY: 0:01 - Link is Up - 100/Full

 

root:/> PHY: 0:01 - Link is Down

 

root:/> dPHY: 0:01 - Link is Up - 100/Full

 

root:/> dhcpcd &

[1] 198 dhcpcd

root:/>

root:/> ifconfig

eth0      Link encap:Ethernet  HWaddr 00:E0:22:FE:42:93

          inet addr:10.99.22.89  Bcast:10.99.22.255  Mask:255.255.255.0

          UP BROADCAST NOTRAILERS RUNNING MULTICAST  MTU:1500  Metric:1

          RX packets:258 errors:0 dropped:6 overruns:0 frame:0

          TX packets:9 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:1000

          RX bytes:36317 (35.4 KiB)  TX bytes:2919 (2.8 KiB)

 

lo        Link encap:Local Loopback

          inet addr:127.0.0.1  Mask:255.0.0.0

          UP LOOPBACK RUNNING  MTU:16436  Metric:1

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:0

          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

 

root:/>

root:/> cat /etc/config/smb.conf

[global]

workgroup = WORKGROUP

encrypt passwords = yes

root:/>

root:/> boa -c /etc &

[2] 204 boa -c /etc

root:/> [03/Jan/1970:01:30:20 +0000] boa: server version Boa/0.94.14rc21

[03/Jan/1970:01:30:20 +0000] boa: server built Nov 10 2011 at 11:10:58.

[03/Jan/1970:01:30:20 +0000] boa: starting server pid=205, port 80

10.99.24.89 - - [03/Jan/1970:01:31:33 +0000] request "GET /favicon.ico HTTP/1.1" ("/home/httpd/www/html/favicon.ico"): document y

10.99.24.89 - - [03/Jan/1970:01:31:33 +0000] request "GET /favicon.ico HTTP/1.1" ("/home/httpd/www/html/favicon.ico"): document y

Mounting the Remote shared directory : //10.99.22.69/music

sh: can't execute 'smbmount': No such file or directory

--

 

Follow-ups

No Messages Were Found

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.config.netaudio    application/octet-stream    52024    Vivi Li

config.linux.netaudio    application/octet-stream    36252    Vivi Li

Outcomes