FAQ: [#6858] Fail to compile bfin_capture.c in trunk after kernel is upgraded to 3.1.0(2011)

Document created by Aaronwu Employee on Sep 12, 2013
Version 1Show Document
  • View in full screen mode

[#6858] Fail to compile bfin_capture.c in trunk after kernel is upgraded to 3.1.0

Submitted By: Vivi Li

Open Date

2011-10-28 04:29:03     Close Date

2012-01-17 00:45:19

Priority:

Medium     Assignee:

Scott Jiang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

Make Errors     Board:

N/A

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3-2011R1-RC2

App binary format:

N/A     

Summary: Fail to compile bfin_capture.c in trunk after kernel is upgraded to 3.1.0

Details:

 

Fail to compile bfin_capture.c in trunk after kernel is upgraded from 3.0.0 to 3.1.0.

 

Last passed version:

--

kernel:    Linux release 3.0.0-ADI-2011R1-pre-svn10099, build #174 Tue Oct 25 19:59:02 CST 2011

toolchain: bfin-uclinux-gcc release gcc version 4.3.5 (ADI-2011R1-RC2)

user-dist: release svn-10452, build #2123 Tue Oct 25 19:57:53 CST 2011

--

 

First failed version:

--

kernel:    Linux release 3.1.0-ADI-2012R1-pre-svn10106, build #180 Thu Oct 27 09:28:12 CST 2011

toolchain: bfin-uclinux-gcc release gcc version 4.3.5 (ADI-2011R1-RC2)

user-dist: release svn-10454, build #2196 Thu Oct 27 09:27:01 CST 2011

--

 

Bellow is the error log:

--

  CC [M]  drivers/media/video/blackfin/bfin_capture.o

drivers/media/video/blackfin/bfin_capture.c: In function ‘bcap_open’:

drivers/media/video/blackfin/bfin_capture.c:192: error: void value not ignored as it ought to be

make[5]: *** [drivers/media/video/blackfin/bfin_capture.o] Error 1

--

 

Follow-ups

 

--- Scott Jiang                                              2011-12-16 04:09:17

fixed.

 

--- Vivi Li                                                  2012-01-17 01:14:00

Close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.camera_vs6624    application/octet-stream    39454    Vivi Li

Attachments

Outcomes