FAQ: [#6839] ubifs issues while updating kernel. 2010r1-rc5 mounted nand(2011)

Document created by Aaronwu Employee on Sep 12, 2013
Version 1Show Document
  • View in full screen mode

[#6839] ubifs issues while updating kernel. 2010r1-rc5 mounted nand

Submitted By: Chris Page

Open Date

2011-10-24 19:46:38     Close Date

2011-10-24 23:45:06

Priority:

Medium High     Assignee:

Nobody

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1-RC5     Release:

2010r1-rc5

Category:

Memory     Board:

Custom

Processor:

BF537     Silicon Revision:

3

Is this bug repeatable?:

Yes     Resolution:

Duplicate

Uboot version or rev.:

2010R1-RC2     Toolchain version or rev.:

4.3.5

App binary format:

FDPIC     

Summary: ubifs issues while updating kernel. 2010r1-rc5 mounted nand

Details:

 

After updating to the later kernel from 2009 I am having many issues with my mounted nand partition Data. It is using ubifs. I have reformatted and cleaned the partition and still get the following output. This partition works great when I use the previous kernel. The error causes the file system to be read only.

 

 

UBI: attaching mtd1 to ubi0

UBI: physical eraseblock size:   131072 bytes (128 KiB)

UBI: logical eraseblock size:    129024 bytes

UBI: smallest flash I/O unit:    2048

UBI: sub-page size:              512

UBI: VID header offset:          512 (aligned 512)

UBI: data offset:                2048

UBI: attached mtd1 to ubi0

UBI: MTD device name:            "Data(nand)"

UBI: MTD device size:            464 MiB

UBI: number of good PEBs:        3711

UBI: number of bad PEBs:         1

UBI: max. allowed volumes:       128

UBI: wear-leveling threshold:    4096

UBI: number of internal volumes: 1

UBI: number of user volumes:     1

UBI: available PEBs:             0

UBI: total number of reserved PEBs: 3711

UBI: number of PEBs reserved for bad PEB handling: 37

UBI: max/mean erase counter: 5/3

UBI: image sequence number: 0

UBI: background thread "ubi_bgt0d" started, PID 250

UBIFS: recovery needed

UBIFS: recovery completed

UBIFS: mounted UBI device 0, volume 0, name "data"

UBIFS: file system size:   471711744 bytes (460656 KiB, 449 MiB, 3656 LEBs)

UBIFS: journal size:       23611392 bytes (23058 KiB, 22 MiB, 183 LEBs)

UBIFS: media format:       w4/r0 (latest is w4/r0)

UBIFS: default compressor: lzo

UBIFS: reserved for root:  4952683 bytes (4836 KiB)

spidev spi0.5: Warning: SPI CPHA not set: Slave Select not under software control!

See Documentation/blackfin/bfin-spi-notes.txt

spidev spi0.5: Warning: SPI CPHA not set: Slave Select not under software control!

See Documentation/blackfin/bfin-spi-notes.txt

spidev spi0.5: Warning: SPI CPHA not set: Slave Select not under software control!

See Documentation/blackfin/bfin-spi-notes.txt

PHY: 0:01 - Link is Up - 100/Full

uncorrectable error :

uncorrectable error :

uncorrectable error :

uncorrectable error :

uncorrectable error :

uncorrectable error :

UBI error: ubi_io_read: error -74 while reading 2836 bytes from PEB 43:73120, read 2836 bytes

UBIFS error (pid 327): try_read_node: cannot read node type 1 from LEB 21:71072, error -74

UBIFS error (pid 327): ubifs_read_node: bad node type (17 but expected 0)

UBIFS error (pid 327): ubifs_read_node: bad node at LEB 15:10056

UBIFS error (pid 327): ubifs_iget: failed to read inode 74, error -22

UBIFS error (pid 327): ubifs_lookup: dead directory entry 'variance.so', error -22

UBIFS warning (pid 327): ubifs_ro_mode: switched to read-only mode, error -22

UBI: scrubbed PEB 2106 (LEB 0:15), data moved to PEB 2107

UBIFS error (pid 327): ubifs_read_node: bad node type (0 but expected 9)

UBIFS error (pid 327): ubifs_read_node: bad node at LEB 14:107304

UBIFS error (pid 327): ubifs_iget: failed to read inode 91, error -22

UBIFS error (pid 327): ubifs_lookup: dead directory entry 'prog2', error -22

UBI: scrubbed PEB 2105 (LEB 0:14), data moved to PEB 2106

uncorrectable error :

uncorrectable error :

UBI error: ubi_io_read: error -74 while reading 160 bytes from PEB 2107:29056, read 160 bytes

UBIFS error (pid 327): ubifs_read_node: bad node type (5 but expected 0)

UBIFS error (pid 327): ubifs_read_node: bad node at LEB 15:27008

UBIFS error (pid 327): ubifs_iget: failed to read inode 92, error -22

UBIFS error (pid 327): ubifs_lookup: dead directory entry 'prog3', error -22

UBIFS error (pid 327): ubifs_check_node: bad magic 0x10183165, expected 0x6101831

UBIFS error (pid 327): ubifs_check_node: bad node at LEB 15:17760

UBIFS error (pid 327): ubifs_read_node: expected node type 0

UBIFS error (pid 327): ubifs_iget: failed to read inode 89, error -117

UBIFS error (pid 327): ubifs_lookup: dead directory entry 'CALIBRATION', error -117

UBI: scrubbed PEB 2107 (LEB 0:15), data moved to PEB 143

spidev spi0.5: Warning: SPI CPHA not set: Slave Select not under software control!

See Documentation/blackfin/bfin-spi-notes.txt

spidev spi0.5: Warning: SPI CPHA not set: Slave Select not under software control!

See Documentation/blackfin/bfin-spi-notes.txt

spidev spi0.5: Warning: SPI CPHA not set: Slave Select not under software control!

See Documentation/blackfin/bfin-spi-notes.txt

UBIFS error (pid 302): make_reservation: cannot reserve 160 bytes in jhead 1, error -30

UBIFS error (pid 302): ubifs_write_inode: can't write inode 87, error -30

UBIFS error (pid 302): make_reservation: cannot reserve 160 bytes in jhead 1, error -30

UBIFS error (pid 302): ubifs_write_inode: can't write inode 88, error -30

UBIFS error (pid 302): make_reservation: cannot reserve 160 bytes in jhead 1, error -30

UBIFS error (pid 302): ubifs_write_inode: can't write inode 84, error -30

UBIFS error (pid 302): make_reservation: cannot reserve 160 bytes in jhead 1, error -30

UBIFS error (pid 302): ubifs_write_inode: can't write inode 89, error -30

 

Follow-ups

No Messages Were Found

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

nandtest.txt    text/plain    180    Chris Page

nandtest.txt    text/plain    180    Chris Page

startup_code.txt    text/plain    13553    Chris Page

bugreport.tar.gz    application/x-gzip    20220    Chris Page

Outcomes