FAQ: [#6728] Duplex fails to work in ad1938 when ADXL34x is attached(2011)

Document created by Aaronwu Employee on Sep 12, 2013
Version 1Show Document
  • View in full screen mode

[#6728] Duplex fails to work in ad1938 when ADXL34x is attached

Submitted By: Vivi Li

Open Date

2011-08-12 03:46:45     Close Date

2011-10-25 01:54:33

Priority:

Medium     Assignee:

Scott Jiang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2011R1     Release:

Category:

N/A     Board:

N/A

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3-2010_Dec_09

App binary format:

N/A     

Summary: Duplex fails to work in ad1938 when ADXL34x is attached

Details:

 

Duplex fails to work in ad1938 when ADXL34x is attached.

This didn't happen in 2010R1.

 

--

Linux version 3.0.0-ADI-2011R1-pre-svn10051 (test@uclinux72-kernel-elf-ad1938) (gcc version 4.3.5 (ADI-trunk/svn-5013) ) #6 Fri 1

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Limiting kernel memory to 56MB due to anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0014b380

  rodata    = 0x0014b380-0x001b629c

  bss       = 0x001b7000-0x001c7328

  data      = 0x001c7328-0x001dc000

    stack   = 0x001da000-0x001dc000

  init      = 0x001dc000-0x008a4000

  available = 0x008a4000-0x03800000

  DMA Zone  = 0x03e00000-0x04000000

Hardware Trace active and enabled

Boot Mode: 0

Blackfin support (C) 2004-2010 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 125 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14224

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50f

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 47888k/65536k RAM, (6944k init code, 1320k kernel code, 580k data, 2048k dma, 6756k reserved)

NR_IRQS:146

Configuring Blackfin Priority Driven Interrupts

bfin-rtc: invalid date; resetting

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Calibrating delay loop... 995.32 BogoMIPS (lpj=1990656)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (35 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

bio: create slab <bio-0> at 0

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs@ffc00500, dma channel@7

Advanced Linux Sound Architecture Driver Version 1.0.24.

Switching to clocksource bfin_cs_cycles

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

debug-mmrs: setting up Blackfin MMR debugfs

msgmni has been set to 93

io scheduler noop registered (default)

bfin-uart: Blackfin serial driver

bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)

bfin_mac bfin_mac.0: eth0: Blackfin on-chip Ethernet MAC driver, Version 1.1

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

bfin-tdm bfin-tdm.0: dma rx:3 tx:4, err irq:45, regs:ffc00800

dma_alloc_init: dma_page @ 0x027fc000 - 512 pages at 0x03e00000

asoc: ad193x-hifi <-> bfin-tdm.0 mapping ok

ALSA device list:

  #0: bfin-ad193x

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-01 06:39:10 UTC (23950)

IP-Config: Gateway not on directly connected network.

Freeing unused kernel memory: 6944k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.18.4 (2011-08-12 09:00:33 CST) hush - the humble shell

 

root:/> PHY: 0:01 - Link is Up - 100/Full

 

root:/>

root:/>

root:/> arecord -t wav -c 2 -f S32_LE -r 48000 -d 15 aaa

Recording WAVE 'aaa' : Signed 32 bit Little Endian, Rate 48000 Hz, Stereo

 

 

root:/>

root:/>

root:/>

root:/> aplay aaa &

[1] 202 aplay aaa

root:/> Playing WAVE 'aaa' : Signed 32 bit Little Endian, Rate 48000 Hz, Stereo

 

root:/>

root:/>

root:/> arecord -t wav -c 2 -f S32_LE -r 48000 -d 5 bbb

Recording WAVE 'bbb' : Signed 32 bit Little Endian, Rate 48000 Hz, Stereo

arecord: pcm_read:1349: read error: Input/output error

root:/> aplay: pcm_write:1268: write error: Input/output error

 

[1] Done                   aplay aaa

root:/>

--

 

Follow-ups

 

--- Scott Jiang                                              2011-09-26 04:10:26

v1.3 board only, you can place ADXL34X with ad1836 together.

 

--- Vivi Li                                                  2011-10-25 02:01:26

ADXL34X is placed in board without ad1938, and both work fine.

Close this bug.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.linux.audio_ad1938    application/octet-stream    36835    Vivi Li

Outcomes