FAQ: [#6603] spi coexistence test fails for not finding /dev/mixer device(2011)

Document created by Aaronwu Employee on Sep 11, 2013
Version 1Show Document
  • View in full screen mode

[#6603] spi coexistence test fails for not finding /dev/mixer device

Submitted By: Mingquan Pan

Open Date

2011-05-17 03:54:51     Close Date

2011-06-01 23:09:54

Priority:

Medium     Assignee:

Scott Jiang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2011R1     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Duplicate

Uboot version or rev.:

    Toolchain version or rev.:

5013

App binary format:

N/A     

Summary: spi coexistence test fails for not finding /dev/mixer device

Details:

 

spi coexistence test fails for not finding /dev/mixer device.

 

BusyBox v1.18.4 (2011-05-16 16:44:09 CST) hush - the humble shell^M

^M

root:/> ^[[6nversionPHY: 0:01 - Link is Up - 100/Full^M

^M

kernel:    Linux release 2.6.39-rc7-ADI-2011R1-pre-svn9883, build #180 Mon May 16 16:48:43 CST 2011^M

toolchain: bfin-linux-uclibc-gcc release gcc version 4.3.5 (ADI-trunk/svn-5013) ^M

user-dist: release svn-10166, build #2543 Mon May 16 16:47:28 CST 2011^M

root:/> ^[successful boot attempt[6n^M

root:/> spawn telnet 10.100.4.50^M

^M

Trying 10.100.4.50...^M^M

Connected to 10.100.4.50.^M^M

Escape character is '^]'.^M^M

^M

^M

^M

BusyBox v1.18.4 (2011-05-16 16:44:09 CST) hush - the humble shell^M

^M

root:/> ^M

root:/> ^[[6nwhile [ 1 ]; do mixer vol 15; mixer vol 20; done^M

/dev/mixer: No such file or directory^M

/dev/mixer: No such file or directory^M

/dev/mixer: No such file or directory^M

/dev/mixer: No such file or directory^M

/dev/mixer: No such file or directory^M

/dev/mixer: No such file or directory^M

 

Follow-ups

 

--- Mike Frysinger                                           2011-06-01 09:23:33

please post the actual config files you're using

 

--- Vivi Li                                                  2011-06-01 23:17:43

Dupe of bug 6619.

Close this one.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes